<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Multiple peripheral data reception in Central in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Multiple-peripheral-data-reception-in-Central/m-p/2140111#M19890</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi Team,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It is mentioned in datasheet that 24 concurrent connections are possible , so is there any use case or any example code in sdk which can explain how a central device can receive data from multiple(more than 2) peripheral devices.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 24 Jul 2025 11:16:49 GMT</pubDate>
    <dc:creator>Chan_17</dc:creator>
    <dc:date>2025-07-24T11:16:49Z</dc:date>
    <item>
      <title>Multiple peripheral data reception in Central</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Multiple-peripheral-data-reception-in-Central/m-p/2140111#M19890</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi Team,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;It is mentioned in datasheet that 24 concurrent connections are possible , so is there any use case or any example code in sdk which can explain how a central device can receive data from multiple(more than 2) peripheral devices.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Jul 2025 11:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Multiple-peripheral-data-reception-in-Central/m-p/2140111#M19890</guid>
      <dc:creator>Chan_17</dc:creator>
      <dc:date>2025-07-24T11:16:49Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple peripheral data reception in Central</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Multiple-peripheral-data-reception-in-Central/m-p/2140296#M19892</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;For running an application that supports multi-paring the most recommended is the Wireless UART example that we provide in the SDK. However for each application we test a number of connections supported without memory or related issues, this will be different in each application. We can see the maximum connections for each application in source/&lt;STRONG&gt;app_preinclude.h&amp;nbsp; --&amp;gt; gAppMaxConnections_c&lt;/STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; (Wireless_uart_freertos for example support 8 in the SDK example)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For complementary information about Multiple Connections in BLE please refer to Chapter 9.10[&lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/_static/wireless/Bluetooth/Bluetooth_Low_Energy_Application_Developer's_Guide.pdf" target="_blank"&gt;Bluetooth Low Energy Application Developer’s Guide&lt;/A&gt;].&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Thu, 24 Jul 2025 17:28:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Multiple-peripheral-data-reception-in-Central/m-p/2140296#M19892</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-07-24T17:28:51Z</dc:date>
    </item>
  </channel>
</rss>