<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: KW45B41Z BLE Set Max Tx Power Failing — Any External Pin Required?</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2124419#M19830</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230059"&gt;@luis_maravilla&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you for the response.&lt;/P&gt;&lt;P&gt;I haven’t made any modifications to the example code from the SDK; I’m using it as provided.&lt;/P&gt;&lt;P&gt;For the setup, I’m using a KW45 EVK with MCU-Link for flashing and debugging. I’m still checking if any additional&lt;STRONG&gt; fuse burning&lt;/STRONG&gt; is required for &lt;STRONG&gt;NBU&lt;/STRONG&gt; usage in EVK , specifically for wireless communication. I’ll go through the Bluetooth Low Energy Demo Applications User’s Guide, as you suggested, and confirm the fuse process accordingly.&lt;/P&gt;&lt;P&gt;Please let me know if there’s anything specific I should look for regarding fuse programming.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Amar&lt;/P&gt;</description>
    <pubDate>Fri, 27 Jun 2025 05:05:52 GMT</pubDate>
    <dc:creator>Amarnath_473</dc:creator>
    <dc:date>2025-06-27T05:05:52Z</dc:date>
    <item>
      <title>KW45B41Z BLE Set Max Tx Power Failing — Any External Pin Required?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2123680#M19826</link>
      <description>&lt;P&gt;I am using the KW45B41Z EVK with the SDK example &lt;STRONG&gt;bluetooth/wireless_uart_freertos&lt;/STRONG&gt;.&amp;nbsp;In the initialization flow, the function &lt;STRONG&gt;PLATFORM_SetBleMaxTxPower()&lt;/STRONG&gt;&amp;nbsp;is failing to set the BLE Tx power.&lt;/P&gt;&lt;P&gt;Is there any external hardware requirement for this to work? Do I need to configure any specific pins (e.g., antenna path control or LDO trim) for proper Tx power configuration on this EVK?&lt;/P&gt;&lt;P&gt;Also, can this API be called immediately after &lt;STRONG&gt;PLATFORM_InitBle()&lt;/STRONG&gt; or should it be called after full BLE stack initialization?&lt;/P&gt;&lt;P&gt;Any suggestions are appreciated.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jun 2025 06:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2123680#M19826</guid>
      <dc:creator>Amarnath_473</dc:creator>
      <dc:date>2025-06-26T06:42:45Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z BLE Set Max Tx Power Failing — Any External Pin Required?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2124190#M19828</link>
      <description>&lt;P&gt;Hello hope you are doing well,&lt;/P&gt;
&lt;P&gt;Could you help us confirm if the code has any modifications from the original in the SDK? And give more description about your set up please?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For external hardware requirement; you will need the NXP IoT Toolbox app in your phone or another KW45 EVK board to interact with.&lt;/P&gt;
&lt;P&gt;I would strongly recommend checking the &lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/_static/wireless/Bluetooth/Bluetooth_Low_Energy_Demo_Applications_User%27s_Guide.pdf" target="_blank"&gt;Bluetooth Low Energy Demo Applications User’s Guide&lt;/A&gt; Chapter 5.12 Wireless UART to follow the steps to run this example.&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jun 2025 17:34:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2124190#M19828</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-06-26T17:34:34Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z BLE Set Max Tx Power Failing — Any External Pin Required?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2124419#M19830</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230059"&gt;@luis_maravilla&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thank you for the response.&lt;/P&gt;&lt;P&gt;I haven’t made any modifications to the example code from the SDK; I’m using it as provided.&lt;/P&gt;&lt;P&gt;For the setup, I’m using a KW45 EVK with MCU-Link for flashing and debugging. I’m still checking if any additional&lt;STRONG&gt; fuse burning&lt;/STRONG&gt; is required for &lt;STRONG&gt;NBU&lt;/STRONG&gt; usage in EVK , specifically for wireless communication. I’ll go through the Bluetooth Low Energy Demo Applications User’s Guide, as you suggested, and confirm the fuse process accordingly.&lt;/P&gt;&lt;P&gt;Please let me know if there’s anything specific I should look for regarding fuse programming.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Amar&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jun 2025 05:05:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2124419#M19830</guid>
      <dc:creator>Amarnath_473</dc:creator>
      <dc:date>2025-06-27T05:05:52Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z BLE Set Max Tx Power Failing — Any External Pin Required?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2124970#M19833</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Thank you for the response.&lt;/P&gt;
&lt;P&gt;There is no need to perform fuse burning in order to use the NBU.&lt;/P&gt;
&lt;P&gt;Could you help us confirm that you followed up the installation of the NBU as the instructions described in Chapter 3.3 in the Getting Started? IF not, I would recommend completing the guide first. &lt;A href="https://www.nxp.com/document/guide/getting-started-with-the-kw45b41z-evaluation-kit:GS-KW45B41ZEVK?_gl=1*sfu24u*_ga*MTE4OTQwMTA4OS4xNzM0NzE4NDY0*_ga_WM5LE0KMSH*czE3NTA5NTQxNjkkbzQ2MiRnMSR0MTc1MDk1NjQzNCRqMjUkbDAkaDUxMDA3ODI4NQ..&amp;amp;section=build-run" target="_blank"&gt;Getting Started with the KW45B41Z Evaluation Kit | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Also, could you help us confirm the following&lt;/P&gt;
&lt;P&gt;What SDK version are you using? What version of MCUXpresso are you using?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jun 2025 20:03:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2124970#M19833</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-06-27T20:03:43Z</dc:date>
    </item>
    <item>
      <title>Re: KW45B41Z BLE Set Max Tx Power Failing — Any External Pin Required?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2125320#M19834</link>
      <description>&lt;P&gt;Hello Luis,&lt;/P&gt;&lt;P&gt;Thank you for the support. After going through the Getting Started guide, I updated the NBU firmware as per the instructions. It is working fine now.&lt;/P&gt;&lt;P&gt;Thanks again for the help.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Amar.&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jun 2025 05:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW45B41Z-BLE-Set-Max-Tx-Power-Failing-Any-External-Pin-Required/m-p/2125320#M19834</guid>
      <dc:creator>Amarnath_473</dc:creator>
      <dc:date>2025-06-30T05:19:59Z</dc:date>
    </item>
  </channel>
</rss>