<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: FRDM-MCXW71 delvelopment board has mal functioning external SW (J12)</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW71-delvelopment-board-has-mal-functioning-external-SW/m-p/2108213#M19748</link>
    <description>&lt;P&gt;Hi Ana,&amp;nbsp; thanks for reply.&lt;BR /&gt;&lt;BR /&gt;After more studying the schematics and documentation.&amp;nbsp; it seems indeed not possible to use this board for debugging to an other external MCU.&lt;BR /&gt;JP12 seems only added to this development board to connect for example the segger J-link to this development board.&lt;BR /&gt;Many other development boards with onboard debug device-iC's&amp;nbsp; do have the posibility to use them as a limited (cheap) debugger and programmer for your own protoype-board.&amp;nbsp; This one from NXP does NOT.&amp;nbsp; thats a big dis advantage.&lt;BR /&gt;Of course I can modify the boards and make the LPC55S69 ready for external use.&amp;nbsp; then I need to patch some connections.&lt;BR /&gt;You can compare this FRDM-MCXW71&amp;nbsp; to the LPC55S69 EVK.&amp;nbsp; that one is able tot use as debuger/programmer.&amp;nbsp; I succeded to us it for the K32W.&lt;BR /&gt;&lt;BR /&gt;If you think I can use this FRDM for external MCU debugging.&amp;nbsp; please explain how.&lt;BR /&gt;So far it will not work, as the local MCU wil disturb SW communication...&lt;BR /&gt;It would have been possible with a very simple change in the design.&amp;nbsp; Just a split in reset...&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 30 May 2025 19:11:04 GMT</pubDate>
    <dc:creator>MVWare</dc:creator>
    <dc:date>2025-05-30T19:11:04Z</dc:date>
    <item>
      <title>FRDM-MCXW71 delvelopment board has mal functioning external SW (J12)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW71-delvelopment-board-has-mal-functioning-external-SW/m-p/2107148#M19741</link>
      <description>&lt;P&gt;I want to use the FRDM-MCXW71&amp;nbsp; development board to debug an external proto board with an K32W041 device.&amp;nbsp; That proto works fine with segger Jlink.&lt;BR /&gt;I dont get SW to work with this FRDM.&lt;BR /&gt;I do not understand from the documentation and schematics, how the local MCXW71 is decoupled, when connecting the external device. On J12 pin 9 will sense the external device, and should switchto that interface. (but FRDM has no coucoupling to the MCXW71, strange! )&lt;BR /&gt;Each time the core is not detected or recognized.&amp;nbsp;&lt;BR /&gt;With the scope I check all signals, all work.&lt;BR /&gt;Cable connection is correct.&lt;BR /&gt;When starting the debug, or flash erase with MCUXpresso, the local MCXW71 stops its ledblinky program, the external device keeps on running its ledblinky program.&amp;nbsp; So it is already wrong that the local MCXW71 is reacting on the debug action. the external should.&lt;BR /&gt;From UM12063, it seems that this FRDm can not debug external devivces, while other NXP documentation sys it can.&amp;nbsp; very confusing.&lt;BR /&gt;I also used a LPC55S69 development board 2 years ago.&amp;nbsp; that was able to program external devices.&amp;nbsp; But is was also equiped with SW disconnection chips..&lt;BR /&gt;Any help or suggestion is welcome..&amp;nbsp; &amp;nbsp;&lt;BR /&gt;Im affrais that NXP has not made a well job on this FRDM board...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 May 2025 12:04:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW71-delvelopment-board-has-mal-functioning-external-SW/m-p/2107148#M19741</guid>
      <dc:creator>MVWare</dc:creator>
      <dc:date>2025-05-29T12:04:54Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MCXW71 delvelopment board has mal functioning external SW (J12)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW71-delvelopment-board-has-mal-functioning-external-SW/m-p/2108194#M19746</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Could you please help me clarify if you wish to use the MCXW71 or the K32W041 as the external debugger?&lt;/P&gt;
&lt;P&gt;Also, could you send me an image of your setup and how you managed the connections?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The available debug scenarios for FRDM-MCXW71 are MCU-Link for debugging the MCXW71 MCU and using an external debugger for debugging the MCXW71 MCU, mentioned on section 3 from the &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM12063" target="_blank"&gt;FRDM-MCXW71 Board User Manual&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ana Sofia.&lt;/P&gt;</description>
      <pubDate>Fri, 30 May 2025 18:41:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW71-delvelopment-board-has-mal-functioning-external-SW/m-p/2108194#M19746</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2025-05-30T18:41:26Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MCXW71 delvelopment board has mal functioning external SW (J12)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW71-delvelopment-board-has-mal-functioning-external-SW/m-p/2108213#M19748</link>
      <description>&lt;P&gt;Hi Ana,&amp;nbsp; thanks for reply.&lt;BR /&gt;&lt;BR /&gt;After more studying the schematics and documentation.&amp;nbsp; it seems indeed not possible to use this board for debugging to an other external MCU.&lt;BR /&gt;JP12 seems only added to this development board to connect for example the segger J-link to this development board.&lt;BR /&gt;Many other development boards with onboard debug device-iC's&amp;nbsp; do have the posibility to use them as a limited (cheap) debugger and programmer for your own protoype-board.&amp;nbsp; This one from NXP does NOT.&amp;nbsp; thats a big dis advantage.&lt;BR /&gt;Of course I can modify the boards and make the LPC55S69 ready for external use.&amp;nbsp; then I need to patch some connections.&lt;BR /&gt;You can compare this FRDM-MCXW71&amp;nbsp; to the LPC55S69 EVK.&amp;nbsp; that one is able tot use as debuger/programmer.&amp;nbsp; I succeded to us it for the K32W.&lt;BR /&gt;&lt;BR /&gt;If you think I can use this FRDM for external MCU debugging.&amp;nbsp; please explain how.&lt;BR /&gt;So far it will not work, as the local MCU wil disturb SW communication...&lt;BR /&gt;It would have been possible with a very simple change in the design.&amp;nbsp; Just a split in reset...&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 30 May 2025 19:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW71-delvelopment-board-has-mal-functioning-external-SW/m-p/2108213#M19748</guid>
      <dc:creator>MVWare</dc:creator>
      <dc:date>2025-05-30T19:11:04Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MCXW71 delvelopment board has mal functioning external SW (J12)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW71-delvelopment-board-has-mal-functioning-external-SW/m-p/2108809#M19754</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You would have to use an external debug probe, you could check the&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcu-link-debug-probe:MCU-LINK" target="_blank"&gt;MCU-Link Debug Probe&lt;/A&gt;&amp;nbsp;and&amp;nbsp;MCU-Link Pro Debug Probe. These are small, economic devices to help debugging and programming.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The MCXW71 can be programmed with the MCU Link, and the MCU-Link Pro supports CMSIS-DAP and/or J-Link protocols.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ana Sofia.&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jun 2025 17:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-MCXW71-delvelopment-board-has-mal-functioning-external-SW/m-p/2108809#M19754</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2025-06-02T17:44:52Z</dc:date>
    </item>
  </channel>
</rss>