<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IW612/IW611 MAYA-W2 Module Bluetooth bring up in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/2107638#M19745</link>
    <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238812"&gt;@nifroidl&lt;/a&gt;&amp;nbsp;In my case when i don't use flow control (RTS unconnected / Module CTS grounded) the interface work. Which hardware connection did you used to make it work?&lt;/P&gt;</description>
    <pubDate>Fri, 30 May 2025 05:18:17 GMT</pubDate>
    <dc:creator>pratham_malaviya</dc:creator>
    <dc:date>2025-05-30T05:18:17Z</dc:date>
    <item>
      <title>IW612/IW611 MAYA-W2 Module Bluetooth bring up</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/1931287#M18655</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I am using the MAYA-W2 module from u-blox for a WiFi Bluetooth Adapter. Since there is the IW611/IW612 populated, maybe some of you can help me. I can easily bring up WiFi using the mwifiex driver and imx-firmware for IW612 but I am not able to bring up Bluetooth:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;root@phyboard-pollux-imx8mp-3:~# hciattach /dev/ttymxc2 any 115200 flow&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Setting TTY to N_HCI line discipline&lt;BR /&gt;Device setup complete&lt;BR /&gt;root@phyboard-pollux-imx8mp-3:~# [ 68.060988] Bluetooth: hci0: command 0x1003 tx timeout&lt;BR /&gt;[ 70.076990] Bluetooth: hci0: command 0x1001 tx timeout&lt;BR /&gt;[ 72.092997] Bluetooth: hci0: command 0x1009 tx timeout&lt;BR /&gt;root@phyboard-pollux-imx8mp-3:~# hciconfig hci0 up&lt;BR /&gt;[ 88.316175] Bluetooth: hci0: command 0x1003 tx timeout&lt;BR /&gt;[ 90.332097] Bluetooth: hci0: command 0x1001 tx timeout&lt;BR /&gt;[ 92.348038] Bluetooth: hci0: command 0x1009 tx timeout&lt;BR /&gt;Can't init device hci0: Connection timed out (110)&lt;BR /&gt;root@phyboard-pollux-imx8mp-3:~# hcitool dev&lt;BR /&gt;Devices:&lt;BR /&gt;&lt;A href="mailto:root@phyboard-pollux-imx8mp-3:~" target="_blank"&gt;root@phyboard-pollux-imx8mp-3:~# &lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Can someone help me? Do you havdthis issue already?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 13 Aug 2024 16:35:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/1931287#M18655</guid>
      <dc:creator>nifroidl</dc:creator>
      <dc:date>2024-08-13T16:35:48Z</dc:date>
    </item>
    <item>
      <title>Re: IW612/IW611 MAYA-W2 Module Bluetooth bring up</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/1931398#M18656</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;I will contact you in the other case.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Aug 2024 18:08:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/1931398#M18656</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2024-08-13T18:08:12Z</dc:date>
    </item>
    <item>
      <title>Re: IW612/IW611 MAYA-W2 Module Bluetooth bring up</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/2107070#M19740</link>
      <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238812"&gt;@nifroidl&lt;/a&gt;&amp;nbsp;,&lt;BR /&gt;Were you able to solve this issue?&lt;BR /&gt;I am stuck at the same.&lt;/P&gt;</description>
      <pubDate>Thu, 29 May 2025 09:59:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/2107070#M19740</guid>
      <dc:creator>pratham_malaviya</dc:creator>
      <dc:date>2025-05-29T09:59:59Z</dc:date>
    </item>
    <item>
      <title>Re: IW612/IW611 MAYA-W2 Module Bluetooth bring up</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/2107507#M19744</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235882"&gt;@pratham_malaviya&lt;/a&gt;&amp;nbsp;Yes. In my case it was an HW issue. I had to switch RTS and CTS signal for UART. After that I was able to get the BT interface running&lt;/P&gt;</description>
      <pubDate>Fri, 30 May 2025 01:28:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/2107507#M19744</guid>
      <dc:creator>nifroidl</dc:creator>
      <dc:date>2025-05-30T01:28:05Z</dc:date>
    </item>
    <item>
      <title>Re: IW612/IW611 MAYA-W2 Module Bluetooth bring up</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/2107638#M19745</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/238812"&gt;@nifroidl&lt;/a&gt;&amp;nbsp;In my case when i don't use flow control (RTS unconnected / Module CTS grounded) the interface work. Which hardware connection did you used to make it work?&lt;/P&gt;</description>
      <pubDate>Fri, 30 May 2025 05:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/2107638#M19745</guid>
      <dc:creator>pratham_malaviya</dc:creator>
      <dc:date>2025-05-30T05:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: IW612/IW611 MAYA-W2 Module Bluetooth bring up</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/2113276#M19768</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/235882"&gt;@pratham_malaviya&lt;/a&gt;&amp;nbsp;Maybe this is your issue. Do you have teh Flow Control Pins available? I think I tried to use the chip without Flow Control and it didn't work.&lt;/P&gt;</description>
      <pubDate>Tue, 10 Jun 2025 06:05:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/IW612-IW611-MAYA-W2-Module-Bluetooth-bring-up/m-p/2113276#M19768</guid>
      <dc:creator>nifroidl</dc:creator>
      <dc:date>2025-06-10T06:05:46Z</dc:date>
    </item>
  </channel>
</rss>