<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic OTA Bootloader Example for MCXW71 in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/OTA-Bootloader-Example-for-MCXW71/m-p/2103879#M19719</link>
    <description>&lt;P&gt;Reading through the&amp;nbsp;Bluetooth® Low Energy Application Developer’s Guide.&lt;/P&gt;&lt;P&gt;There should be an example project that implements OTA BLE through a bootloader.&lt;/P&gt;&lt;P&gt;The OTAP Bootloader project and source code can be found in the \boards\&amp;lt;board&amp;gt;\wireless_examples\framework\bootloader_otap\ folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does this example exist for the MCXW71 / KW45 chips?&lt;/P&gt;&lt;P&gt;Which SDK would have this example that could be most easily ported?&lt;/P&gt;</description>
    <pubDate>Sun, 25 May 2025 16:54:17 GMT</pubDate>
    <dc:creator>VeridianJack</dc:creator>
    <dc:date>2025-05-25T16:54:17Z</dc:date>
    <item>
      <title>OTA Bootloader Example for MCXW71</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/OTA-Bootloader-Example-for-MCXW71/m-p/2103879#M19719</link>
      <description>&lt;P&gt;Reading through the&amp;nbsp;Bluetooth® Low Energy Application Developer’s Guide.&lt;/P&gt;&lt;P&gt;There should be an example project that implements OTA BLE through a bootloader.&lt;/P&gt;&lt;P&gt;The OTAP Bootloader project and source code can be found in the \boards\&amp;lt;board&amp;gt;\wireless_examples\framework\bootloader_otap\ folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does this example exist for the MCXW71 / KW45 chips?&lt;/P&gt;&lt;P&gt;Which SDK would have this example that could be most easily ported?&lt;/P&gt;</description>
      <pubDate>Sun, 25 May 2025 16:54:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/OTA-Bootloader-Example-for-MCXW71/m-p/2103879#M19719</guid>
      <dc:creator>VeridianJack</dc:creator>
      <dc:date>2025-05-25T16:54:17Z</dc:date>
    </item>
    <item>
      <title>Re: OTA Bootloader Example for MCXW71</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/OTA-Bootloader-Example-for-MCXW71/m-p/2104574#M19723</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;To use the OTAP Bootloader I would recommend using the &lt;STRONG&gt;KW45B41Z-EVK&lt;/STRONG&gt; SDK Most Recent Version (25.03.00), the example you'll need to implement is the &lt;STRONG&gt;[otap_client_att_freertos]&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I would recommend checking the Bluetooth Low Energy Demo Applications User’s Guide Chapter 5.11 for further information about OTAP in KW45. &lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/_static/wireless/Bluetooth/Bluetooth_Low_Energy_Demo_Applications_User%27s_Guide.pdf" target="_blank"&gt;Bluetooth Low Energy Demo Applications User’s Guide&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, This Application note can be useful regarding the KW45 OTAP bootloader &lt;A href="https://www.nxp.com/docs/en/application-note/AN13860.pdf" target="_blank"&gt;Creating Firmware Update Image for KW45B41Z/K32W148 using Over the Air Programming Tool&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Mon, 26 May 2025 17:45:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/OTA-Bootloader-Example-for-MCXW71/m-p/2104574#M19723</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-05-26T17:45:13Z</dc:date>
    </item>
  </channel>
</rss>