<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic UART debug output on PNEV5180B in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/UART-debug-output-on-PNEV5180B/m-p/2091335#M19694</link>
    <description>&lt;P&gt;I am trying to enable debug logs over UART on the evaluation board I have (PNEV5180B)&lt;/P&gt;&lt;P&gt;Unfortunately, I didn't find any schematics for the board, so I made some assumptions. The first one is that J201 is a UART port connected to the ARM MCU. Taking into account that it has 3 pins marked as TX, RX and Ground I think it is quite plausible.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then I've checked how the work with UART was implemented in&amp;nbsp;lpcopen lpcxpresso SDK for lpc1769 and did the same. I managed to make all related IRQ triggers, and I believe smth is transferred, but I still can't manage to get any data on the pins themselves. They just keep silent (not noise, just silence). I've tried all 3 UARTs, they stay the same.&lt;/P&gt;&lt;P&gt;So the questions are:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;- Is J201 actually an UART?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;- Which UART port does it correspond to?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;- Are there any functional examples of using UART communication with&amp;nbsp;PNEV5180B boards?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 05 May 2025 09:47:24 GMT</pubDate>
    <dc:creator>henry_pootle</dc:creator>
    <dc:date>2025-05-05T09:47:24Z</dc:date>
    <item>
      <title>UART debug output on PNEV5180B</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/UART-debug-output-on-PNEV5180B/m-p/2091335#M19694</link>
      <description>&lt;P&gt;I am trying to enable debug logs over UART on the evaluation board I have (PNEV5180B)&lt;/P&gt;&lt;P&gt;Unfortunately, I didn't find any schematics for the board, so I made some assumptions. The first one is that J201 is a UART port connected to the ARM MCU. Taking into account that it has 3 pins marked as TX, RX and Ground I think it is quite plausible.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then I've checked how the work with UART was implemented in&amp;nbsp;lpcopen lpcxpresso SDK for lpc1769 and did the same. I managed to make all related IRQ triggers, and I believe smth is transferred, but I still can't manage to get any data on the pins themselves. They just keep silent (not noise, just silence). I've tried all 3 UARTs, they stay the same.&lt;/P&gt;&lt;P&gt;So the questions are:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;- Is J201 actually an UART?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;- Which UART port does it correspond to?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;- Are there any functional examples of using UART communication with&amp;nbsp;PNEV5180B boards?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 May 2025 09:47:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/UART-debug-output-on-PNEV5180B/m-p/2091335#M19694</guid>
      <dc:creator>henry_pootle</dc:creator>
      <dc:date>2025-05-05T09:47:24Z</dc:date>
    </item>
  </channel>
</rss>