<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KW0x- Generating a continuous un-modulated signal in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/KW0x-Generating-a-continuous-un-modulated-signal/m-p/367078#M196</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Generating a Continuous Un-modulated signal is a common request for customers evaluating RF performance.&lt;/P&gt;&lt;P&gt;This allows the user to measure not only the accuracy of the transmission's center frequency but it is also useful &lt;/P&gt;&lt;P&gt;to measure power consumption. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To generate this signal the following steps are needed:&lt;/P&gt;&lt;P&gt;1) Set Data Mode to "Data Mode Continuous"&lt;/P&gt;&lt;P&gt;RegDataModul(0x02) &lt;/P&gt;&lt;P&gt;DATA MODE -&amp;gt;&amp;nbsp; Continuous mode (any: with or without bit syncrhonizer)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Set Fdev to zero&lt;/P&gt;&lt;P&gt;RegFdevMsb (0x05)= 0x00&lt;/P&gt;&lt;P&gt;RegFdevLsb (0x06)= 0x00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) Put xcvr in TX mode&lt;/P&gt;&lt;P&gt;RegOpMode (0x01)&lt;/P&gt;&lt;P&gt;MODE -&amp;gt; 011 (Transmitter mode- TX)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM style=": ; color: #575757; text-decoration: underline;"&gt;Code Snippet example (SMAC-based):&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Set Data Mode*/&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PhyPib_SetDataMode(DataModul_DataMode_Continous);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Set Fdev to zero*/&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PhyPib_SetFreqDeviation(0x00); &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Put transceiver in TX mode */&lt;/P&gt;&lt;P&gt; &lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PhyPib_SetOperationMode (OpMode_Transmitter);&amp;nbsp; &lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 03 Oct 2014 18:56:55 GMT</pubDate>
    <dc:creator>CesarM</dc:creator>
    <dc:date>2014-10-03T18:56:55Z</dc:date>
    <item>
      <title>KW0x- Generating a continuous un-modulated signal</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW0x-Generating-a-continuous-un-modulated-signal/m-p/367078#M196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Generating a Continuous Un-modulated signal is a common request for customers evaluating RF performance.&lt;/P&gt;&lt;P&gt;This allows the user to measure not only the accuracy of the transmission's center frequency but it is also useful &lt;/P&gt;&lt;P&gt;to measure power consumption. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To generate this signal the following steps are needed:&lt;/P&gt;&lt;P&gt;1) Set Data Mode to "Data Mode Continuous"&lt;/P&gt;&lt;P&gt;RegDataModul(0x02) &lt;/P&gt;&lt;P&gt;DATA MODE -&amp;gt;&amp;nbsp; Continuous mode (any: with or without bit syncrhonizer)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) Set Fdev to zero&lt;/P&gt;&lt;P&gt;RegFdevMsb (0x05)= 0x00&lt;/P&gt;&lt;P&gt;RegFdevLsb (0x06)= 0x00&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) Put xcvr in TX mode&lt;/P&gt;&lt;P&gt;RegOpMode (0x01)&lt;/P&gt;&lt;P&gt;MODE -&amp;gt; 011 (Transmitter mode- TX)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM style=": ; color: #575757; text-decoration: underline;"&gt;Code Snippet example (SMAC-based):&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Set Data Mode*/&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PhyPib_SetDataMode(DataModul_DataMode_Continous);&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*Set Fdev to zero*/&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PhyPib_SetFreqDeviation(0x00); &lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Put transceiver in TX mode */&lt;/P&gt;&lt;P&gt; &lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PhyPib_SetOperationMode (OpMode_Transmitter);&amp;nbsp; &lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Oct 2014 18:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW0x-Generating-a-continuous-un-modulated-signal/m-p/367078#M196</guid>
      <dc:creator>CesarM</dc:creator>
      <dc:date>2014-10-03T18:56:55Z</dc:date>
    </item>
  </channel>
</rss>