<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: No Response from JN5179 in Bootloader mode for Read Flash ID Command in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2060125#M19567</link>
    <description>Hi Luis,&lt;BR /&gt;&lt;BR /&gt;As mentioned in JN-AN-1003.pdf, Serial communication between the PC and boot loader is implemented as 8,N,1,38K4 from the JN514x/JN5139 UART 0.&lt;BR /&gt;&lt;BR /&gt;I was using UART1 so it is causing the issue.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Rajani Sureja</description>
    <pubDate>Wed, 12 Mar 2025 06:42:57 GMT</pubDate>
    <dc:creator>rajanisureja1</dc:creator>
    <dc:date>2025-03-12T06:42:57Z</dc:date>
    <item>
      <title>No Response from JN5179 in Bootloader mode for Read Flash ID Command</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2058745#M19562</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Hi Support Team,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am using the &lt;STRONG&gt;JN5179&lt;/STRONG&gt; chipset and attempting to download firmware via the &lt;STRONG&gt;UART interface&lt;/STRONG&gt; using the built-in bootloader. I am following the &lt;STRONG&gt;JN-AN-1003&lt;/STRONG&gt; document to achieve this and have configured the UART to &lt;STRONG&gt;38400 baud&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;As per the message sequence, I am sending the &lt;STRONG&gt;Read Flash ID request&lt;/STRONG&gt;, which consists of &lt;STRONG&gt;3 bytes&lt;/STRONG&gt;, after putting the JN5179 into &lt;STRONG&gt;bootloader mode&lt;/STRONG&gt;:&lt;/P&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;0&lt;/SPAN&gt;x02 (Length), &lt;SPAN class=""&gt;0&lt;/SPAN&gt;x25 (Message Type), &lt;SPAN class=""&gt;0&lt;/SPAN&gt;x27 (Checksum)&lt;/SPAN&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;P&gt;However, I am &lt;STRONG&gt;not receiving any response&lt;/STRONG&gt; from the bootloader for this command. Could you please help me understand why the JN5179 is not responding and suggest possible solutions?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Thanks &amp;amp; Regards,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Rajani Sureja&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Mar 2025 12:25:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2058745#M19562</guid>
      <dc:creator>rajanisureja1</dc:creator>
      <dc:date>2025-03-10T12:25:33Z</dc:date>
    </item>
    <item>
      <title>Re: No Response from JN5179 in Bootloader mode for Read Flash ID Command</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2058948#M19563</link>
      <description>&lt;P&gt;Hello Rajani&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you using an NXP Module for this application?&lt;/P&gt;
&lt;P&gt;Can you send another command through the bootloader and get a response? Or&lt;/P&gt;
&lt;P&gt;Is this the only bootloader command that you can't get a response?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Mon, 10 Mar 2025 18:26:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2058948#M19563</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-03-10T18:26:03Z</dc:date>
    </item>
    <item>
      <title>Re: No Response from JN5179 in Bootloader mode for Read Flash ID Command</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2059208#M19564</link>
      <description>&lt;P&gt;&lt;STRONG&gt;Hi Luis,&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I am using an &lt;STRONG&gt;ESP32&lt;/STRONG&gt; as the host controller, with a &lt;STRONG&gt;JN5179&lt;/STRONG&gt; connected to it.&lt;/P&gt;&lt;P&gt;I am able to successfully send other commands to the JN5179 in &lt;STRONG&gt;normal mode&lt;/STRONG&gt; (not in bootloader mode) — such as creating a Zigbee network, channel selection, reading device information, etc. — without any issues, so the serial connection appears to be working correctly.&lt;/P&gt;&lt;P&gt;However, I am &lt;STRONG&gt;not receiving any response&lt;/STRONG&gt; when sending commands in &lt;STRONG&gt;bootloader mode&lt;/STRONG&gt;. I need to deploy the firmware over UART in bootloader mode, but the JN5179 does not seem to respond.&lt;/P&gt;&lt;P&gt;Could you please help me identify what might be causing this issue?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Thanks &amp;amp; Regards,&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Rajani Sureja&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Mar 2025 05:43:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2059208#M19564</guid>
      <dc:creator>rajanisureja1</dc:creator>
      <dc:date>2025-03-11T05:43:50Z</dc:date>
    </item>
    <item>
      <title>Re: No Response from JN5179 in Bootloader mode for Read Flash ID Command</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2060110#M19566</link>
      <description>Hi Luis,&lt;BR /&gt;&lt;BR /&gt;Can you please confirm which UART number/pins of JN5179 the bootloader will accept commands from? It seems there might be an issue with the JN UART I'm using to send commands in bootloader mode.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Rajani Sureja</description>
      <pubDate>Wed, 12 Mar 2025 06:31:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2060110#M19566</guid>
      <dc:creator>rajanisureja1</dc:creator>
      <dc:date>2025-03-12T06:31:57Z</dc:date>
    </item>
    <item>
      <title>Re: No Response from JN5179 in Bootloader mode for Read Flash ID Command</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2060125#M19567</link>
      <description>Hi Luis,&lt;BR /&gt;&lt;BR /&gt;As mentioned in JN-AN-1003.pdf, Serial communication between the PC and boot loader is implemented as 8,N,1,38K4 from the JN514x/JN5139 UART 0.&lt;BR /&gt;&lt;BR /&gt;I was using UART1 so it is causing the issue.&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Rajani Sureja</description>
      <pubDate>Wed, 12 Mar 2025 06:42:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/No-Response-from-JN5179-in-Bootloader-mode-for-Read-Flash-ID/m-p/2060125#M19567</guid>
      <dc:creator>rajanisureja1</dc:creator>
      <dc:date>2025-03-12T06:42:57Z</dc:date>
    </item>
  </channel>
</rss>