<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: K32W041 - read configuration from memory dump</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2053165#M19528</link>
    <description>Thank you for your answer. I know that there are examples of how to prepare the appropriate firmware with support for Thread.&lt;BR /&gt;&lt;BR /&gt;I wonder if it is possible to read the current configuration(pins, clocks), for example, using MCUXpresso?&lt;BR /&gt;The problem is that the system is connected directly to the SoC, but I don't know, for example, which GPIOs were used.</description>
    <pubDate>Thu, 27 Feb 2025 17:25:17 GMT</pubDate>
    <dc:creator>hres</dc:creator>
    <dc:date>2025-02-27T17:25:17Z</dc:date>
    <item>
      <title>K32W041 - read configuration from memory dump</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2049147#M19508</link>
      <description>&lt;DIV class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I have a board with integrated K32W041 chip but I don't know how it's configured.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Communication is possible via UART.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Is it possible to read the pin and clock configuration from memory dumps made with dk6prog?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;Regards,&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Fri, 21 Feb 2025 15:01:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2049147#M19508</guid>
      <dc:creator>hres</dc:creator>
      <dc:date>2025-02-21T15:01:21Z</dc:date>
    </item>
    <item>
      <title>Re: K32W041 - read configuration from memory dump</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2049239#M19509</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;Are you working with a development kit? Or is it a custom board?&lt;/P&gt;
&lt;P&gt;Can you comment on what application did you flashed on the chip?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Luis&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 18:08:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2049239#M19509</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-02-21T18:08:37Z</dc:date>
    </item>
    <item>
      <title>Re: K32W041 - read configuration from memory dump</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2049260#M19510</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;This is a custom board.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Currently there is a firmware that allows to configure it from phone on first start.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I would like to prepare firmware with Thread support and run Thread Boarder Router.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Info from dk6prog:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;PRE&gt;Chip ID: 0x88888888
ROM Version: 0x140000cc
MAC Address: xx:xx:xx:xx:xx:xx:xx:xx

Detected DEVICE: K32W041

  Memory   Memory ID   Base Address   Length    Sector Size   Memory Type   Access            
----------------------------------------------------------------------------------------------
  FLASH    0           0x0            0x9de00   0x200         FLASH         All is available  
  PSECT    1           0x0            0x1e0     0x10          FLASH         All is available  
  pFLASH   2           0x0            0x1e0     0x10          FLASH         All is available  
  Config   3           0x9fc00        0x200     0x200         FLASH         All is available  
  EFUSE    4           0x0            0x80      0x2           EFUSE (OTP)   Write Enabled     
  ROM      5           0x3000000      0x20000   0x1           ROM           Write Enabled     
  RAM0     6           0x4000000      0x16000   0x1           RAM           Write Enabled     
  RAM1     7           0x4020000      0x10000   0x1           RAM           Write Enabled&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 21 Feb 2025 19:11:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2049260#M19510</guid>
      <dc:creator>hres</dc:creator>
      <dc:date>2025-02-21T19:11:45Z</dc:date>
    </item>
    <item>
      <title>Re: K32W041 - read configuration from memory dump</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2050243#M19515</link>
      <description>&lt;P lang="es-MX"&gt;For testing Thread examples and more information about commands please refer to NXP Github&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;"&gt;&lt;A href="https://github.com/NXP/ot-nxp" target="_blank"&gt;&lt;SPAN&gt;GitHub - NXP/ot-nxp: OpenThread on NXP examples.&lt;/SPAN&gt;&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Feb 2025 21:47:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2050243#M19515</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-02-24T21:47:24Z</dc:date>
    </item>
    <item>
      <title>Re: K32W041 - read configuration from memory dump</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2053165#M19528</link>
      <description>Thank you for your answer. I know that there are examples of how to prepare the appropriate firmware with support for Thread.&lt;BR /&gt;&lt;BR /&gt;I wonder if it is possible to read the current configuration(pins, clocks), for example, using MCUXpresso?&lt;BR /&gt;The problem is that the system is connected directly to the SoC, but I don't know, for example, which GPIOs were used.</description>
      <pubDate>Thu, 27 Feb 2025 17:25:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2053165#M19528</guid>
      <dc:creator>hres</dc:creator>
      <dc:date>2025-02-27T17:25:17Z</dc:date>
    </item>
    <item>
      <title>Re: K32W041 - read configuration from memory dump</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2055696#M19547</link>
      <description>Hi&lt;BR /&gt;No, it's not possible to read, The GPIOs/CLK should be declared in the programming code.&lt;BR /&gt;&lt;BR /&gt;Best Regards</description>
      <pubDate>Tue, 04 Mar 2025 17:40:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2055696#M19547</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-03-04T17:40:24Z</dc:date>
    </item>
    <item>
      <title>Re: K32W041 - read configuration from memory dump</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2055751#M19548</link>
      <description>Thank you for your answer. I'm afraid that if I use the firmware from the example I will lose contact with the chip.&lt;BR /&gt;&lt;BR /&gt;Are there sources for the "NXP K32W Device Programmer" application available somewhere?</description>
      <pubDate>Tue, 04 Mar 2025 20:25:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/K32W041-read-configuration-from-memory-dump/m-p/2055751#M19548</guid>
      <dc:creator>hres</dc:creator>
      <dc:date>2025-03-04T20:25:20Z</dc:date>
    </item>
  </channel>
</rss>