<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: kw45 be stuck at Host_Task</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2040259#M19496</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;I modified it on the w_uart example project, the Bluetooth part of the chance is unchanged, only added a few tasks, the recurrence probability of this problem is very low, need to connect many times to be repeated, hope to give some suggestions, not necessarily in the example project to solve the problem, should all developers will modify the example project for development!&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; sdk version is 2.12.7. Thank you!&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 08 Feb 2025 02:04:48 GMT</pubDate>
    <dc:creator>wjw2026</dc:creator>
    <dc:date>2025-02-08T02:04:48Z</dc:date>
    <item>
      <title>kw45 be stuck at Host_Task</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2039851#M19492</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The KW45 runs in slave mode, and the Android phone app repeatedly disconnects the connection, and occasionally the kw45 is stuck, which does not occur at the time of connection and disconnection, but several seconds or tens of seconds after the connection is successful.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Debugging analysis found that,kw45 be stuck at Host_Task,o&lt;/SPAN&gt;ther tasks cannot run.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The following is a screenshot of the task running. Repeatedly running the screenshot is&amp;nbsp;Host_Task&lt;/SPAN&gt;&lt;/P&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="1.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/322865iD55F0B14E15368A7/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;Please technical guidance, thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 09:30:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2039851#M19492</guid>
      <dc:creator>wjw2026</dc:creator>
      <dc:date>2025-02-07T09:30:10Z</dc:date>
    </item>
    <item>
      <title>Re: kw45 be stuck at Host_Task</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2039858#M19493</link>
      <description>&lt;P class=""&gt;Provide partial map files:&lt;/P&gt;&lt;P class=""&gt;.bss.pxCurrentTCB&lt;BR /&gt;0x2000319c 0x4 ./freertos/freertos_kernel/tasks.o&lt;BR /&gt;0x2000319c pxCurrentTCB&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;.text.PLATFORM_LoadHwParams&lt;BR /&gt;0x0004710e 0x26 ./framework/Platform/fwk_platform.o&lt;BR /&gt;0x0004710e PLATFORM_LoadHwParams&lt;BR /&gt;.text.PLATFORM_GetMaxTimeStamp&lt;BR /&gt;0x00047134 0xa ./framework/Platform/fwk_platform.o&lt;BR /&gt;0x00047134 PLATFORM_GetMaxTimeStamp&lt;BR /&gt;.text.PLATFORM_IsTimeoutExpired&lt;BR /&gt;0x0004713e 0x44 ./framework/Platform/fwk_platform.o&lt;BR /&gt;0x0004713e PLATFORM_IsTimeoutExpired&lt;BR /&gt;.text.PLATFORM_WaitTimeout&lt;BR /&gt;0x00047182 0x1c ./framework/Platform/fwk_platform.o&lt;BR /&gt;0x00047182 PLATFORM_WaitTimeout&lt;BR /&gt;.text.PLATFORM_Delay&lt;BR /&gt;0x0004719e 0x14 ./framework/Platform/fwk_platform.o&lt;BR /&gt;0x0004719e PLATFORM_Delay&lt;BR /&gt;.text.mcmgr_imu_remote_active_rel&lt;BR /&gt;0x000471b2 0x8 ./framework/Platform/fwk_platform.o&lt;BR /&gt;0x000471b2 mcmgr_imu_remote_active_rel&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 09:39:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2039858#M19493</guid>
      <dc:creator>wjw2026</dc:creator>
      <dc:date>2025-02-07T09:39:04Z</dc:date>
    </item>
    <item>
      <title>Re: kw45 be stuck at Host_Task</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2040125#M19495</link>
      <description>&lt;P&gt;Hi can you provide more details about your situation please,&lt;/P&gt;
&lt;P&gt;What example are you running?&lt;/P&gt;
&lt;P&gt;What version of MCUXpresso are you using?&lt;/P&gt;
&lt;P&gt;Are you using the KW45B1Z-EVK or a custom board?&lt;/P&gt;
&lt;P&gt;Do you have any other modifications on your code?&lt;/P&gt;
&lt;P lang="es-MX"&gt;Are you using a phone app from NXP?&lt;/P&gt;</description>
      <pubDate>Fri, 07 Feb 2025 17:35:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2040125#M19495</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-02-07T17:35:09Z</dc:date>
    </item>
    <item>
      <title>Re: kw45 be stuck at Host_Task</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2040259#M19496</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;I modified it on the w_uart example project, the Bluetooth part of the chance is unchanged, only added a few tasks, the recurrence probability of this problem is very low, need to connect many times to be repeated, hope to give some suggestions, not necessarily in the example project to solve the problem, should all developers will modify the example project for development!&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; sdk version is 2.12.7. Thank you!&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 08 Feb 2025 02:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2040259#M19496</guid>
      <dc:creator>wjw2026</dc:creator>
      <dc:date>2025-02-08T02:04:48Z</dc:date>
    </item>
    <item>
      <title>Re: kw45 be stuck at Host_Task</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2043627#M19504</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;NXP has the "NXP IoT Toolbox app" for testing this Wireless example, I would recommend using this instead.&lt;/P&gt;
&lt;P&gt;The first thing I'd check is if there are enough resources for the new tasks.&lt;/P&gt;
&lt;P&gt;Could it be possible that miss to allocate resources for the new tasks, and then the Host_Task is stuck?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also for recommendations and explanations on functions, you can consult the BLE Application Developer's Guide &lt;A href="https://mcuxpresso.nxp.com/mcuxsdk/latest/html/_static/wireless/Bluetooth/Bluetooth_Low_Energy_Application_Developer's_Guide.pdf" target="_blank"&gt;Bluetooth Low Energy Application Developer’s Guide&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;This document explains how to integrate Task Priority relating to Host Task Initialization and provides more explanations about task and event queues. Chapter 3, and Chapter 9.5.2&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Have a great day&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards Luis&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 13 Feb 2025 17:27:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/kw45-be-stuck-at-Host-Task/m-p/2043627#M19504</guid>
      <dc:creator>luis_maravilla</dc:creator>
      <dc:date>2025-02-13T17:27:30Z</dc:date>
    </item>
  </channel>
</rss>