<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックOne-time NFC program downloader.</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/One-time-NFC-program-downloader/m-p/1966346#M19018</link>
    <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I'm working on a project with the NHS3100, where the device should not be constantly powered. The goal is for it to read the temperature from its sensor and expose it as a parameter in a URL, which will be published on the NFC tag.&lt;/P&gt;&lt;P&gt;I successfully uploaded the code using J-Link in MCUXpresso, and everything works perfectly. However, when I upload the code using the NHS31xx NFC Program Loader, the code uploads fine, but my phone no longer reads the tag unless the tag is externally powered.&lt;/P&gt;&lt;P&gt;What configuration do I need to enable the NFC tag to be powered through NFC after uploading the code via NFC Program Loader?&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated!&lt;/P&gt;</description>
    <pubDate>Thu, 03 Oct 2024 11:01:25 GMT</pubDate>
    <dc:creator>gpol2003</dc:creator>
    <dc:date>2024-10-03T11:01:25Z</dc:date>
    <item>
      <title>One-time NFC program downloader.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/One-time-NFC-program-downloader/m-p/1966346#M19018</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I'm working on a project with the NHS3100, where the device should not be constantly powered. The goal is for it to read the temperature from its sensor and expose it as a parameter in a URL, which will be published on the NFC tag.&lt;/P&gt;&lt;P&gt;I successfully uploaded the code using J-Link in MCUXpresso, and everything works perfectly. However, when I upload the code using the NHS31xx NFC Program Loader, the code uploads fine, but my phone no longer reads the tag unless the tag is externally powered.&lt;/P&gt;&lt;P&gt;What configuration do I need to enable the NFC tag to be powered through NFC after uploading the code via NFC Program Loader?&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated!&lt;/P&gt;</description>
      <pubDate>Thu, 03 Oct 2024 11:01:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/One-time-NFC-program-downloader/m-p/1966346#M19018</guid>
      <dc:creator>gpol2003</dc:creator>
      <dc:date>2024-10-03T11:01:25Z</dc:date>
    </item>
    <item>
      <title>Re: One-time NFC program downloader.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/One-time-NFC-program-downloader/m-p/1966626#M19020</link>
      <description>&lt;P lang="en-US"&gt;Hello, my name is Fabian, I've been assigned to support your case.&lt;/P&gt;
&lt;P lang="en-US"&gt;Thank you for your interest in our products&lt;/P&gt;
&lt;P lang="en-US"&gt;The NHS3100 has a VNFC which is a power input selector that is in charge of selecting the switch that fulfills the PMU requirements.&lt;/P&gt;
&lt;P lang="en-US"&gt;For further information please take a look at section &lt;A href="https://www.nxp.com/docs/en/data-sheet/NHS3100.pdf" target="_self"&gt;8.4.1 System power architecture&lt;/A&gt; where the VNFC and NFC Power Switch (PSWNFC) are explained and shown in a diagram.&lt;/P&gt;
&lt;P lang="en-US"&gt;Please also take a look at &lt;STRONG&gt;UM10876&lt;/STRONG&gt; 5.4 System power architecture where the power configurations and, sequences are also described.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Oct 2024 22:22:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/One-time-NFC-program-downloader/m-p/1966626#M19020</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2024-10-03T22:22:03Z</dc:date>
    </item>
  </channel>
</rss>