<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GENFSK can't monitor ios rssi in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1865804#M17435</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;SPAN&gt;while having via CAN 4 KW35 units that are receiving information form the KW38 connection.&amp;nbsp;&lt;FONT color="#000000"&gt;&amp;nbsp;Actually,&amp;nbsp; the four monitoring devices are kw36.&amp;nbsp; And yes the four kw36 all running gfsk to get RSSI between cellphone and kw38. In order to accomplish ranging test in vehicle.&amp;nbsp;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;SPAN&gt;&lt;FONT color="#000000"&gt;But It doesn't work when I were using iphone, I've tried iphone 15 pro, iphone 13 etc.&amp;nbsp;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;Also can you please share with me on a more detailed way how are you running the connectivity test (GenFSK) project.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;SPAN&gt;After I connect my Android phone to the KW38, it conveys parameters such as hopIncrement, crcSeed, syncAddress, connection interval, and channel map to the KW36 device via CAN. Once the XCVR_GENFSK_ENABLED and related features are enabled on the KW36, the GENFSK_InterruptHandler interrupt callback can detect the masterRSSI and slaveRSSI. This process is seamless when I use my Android phone. However, when I switch to an iPhone, the conditional check &lt;/SPAN&gt;if (irqStatus &amp;amp; GENFSK_IRQ_CTRL_RX_IRQ_MASK)&lt;SPAN&gt; doesn't seem to be triggered, suggesting that packets may not be captured. The access address and crcSeed I transmit to the KW36 appear to be correct upon inspection, and there are no obvious anomalies. Could you shed light on what might be causing this issue?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 15 May 2024 02:06:02 GMT</pubDate>
    <dc:creator>darkblue</dc:creator>
    <dc:date>2024-05-15T02:06:02Z</dc:date>
    <item>
      <title>GENFSK can't monitor ios rssi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1864409#M17398</link>
      <description>&lt;P&gt;Hi Tech,&lt;/P&gt;&lt;P&gt;I use genfsk module to monitor RSSI of BLE.&amp;nbsp; When I use iphone 15 to connect KW36, then the other KW36 devices can't get RSSI. But when I use Huawei meta 30pro then it works.&lt;/P&gt;&lt;P&gt;My device&lt;/P&gt;</description>
      <pubDate>Mon, 13 May 2024 12:02:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1864409#M17398</guid>
      <dc:creator>darkblue</dc:creator>
      <dc:date>2024-05-13T12:02:26Z</dc:date>
    </item>
    <item>
      <title>Re: GENFSK can't monitor ios rssi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1864410#M17399</link>
      <description>My device is KW36, and SDK is 2.2.10</description>
      <pubDate>Mon, 13 May 2024 12:03:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1864410#M17399</guid>
      <dc:creator>darkblue</dc:creator>
      <dc:date>2024-05-13T12:03:27Z</dc:date>
    </item>
    <item>
      <title>Re: GENFSK can't monitor ios rssi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1864779#M17410</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP support.&lt;/P&gt;
&lt;P&gt;I appreciate the details related to SDK and the board you are using can you please help me confirm if this is an EVK.&lt;/P&gt;
&lt;P&gt;Also I understand that the problem is involved when using an Iphone can you please share with me how are you performing this test? So we can reproduce this test case. I think for the type of testing that you are using the connectivity test (GenFSK) and using the Range Test case.&lt;/P&gt;
&lt;P&gt;Can you please confirm this and give more details o how yo are testing this. Also I do recommend to use a latest version of this &lt;A title="SDK 2.2.12" href="https://mcuxpresso.nxp.com/en/builder?hw=FRDM-KW36" target="_blank" rel="noopener"&gt;SDK 2.2.12&lt;/A&gt;.&lt;/P&gt;</description>
      <pubDate>Mon, 13 May 2024 23:12:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1864779#M17410</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2024-05-13T23:12:03Z</dc:date>
    </item>
    <item>
      <title>Re: GENFSK can't monitor ios rssi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1864829#M17412</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I use a KW38 as a peripheral, and then connect it to four KW36 units via CAN. After connecting an Android phone to the KW38, I obtained the related listening information for genfsk as shown in the figure below.&amp;nbsp;The four KW36 units can obtain the masterRSSI, which I believe refers to the Received Signal Strength Indicator (RSSI) of the heartbeat packets from the Android phone.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="darkblue_0-1715650884753.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/278541iCD9B43620E5938DB/image-size/medium?v=v2&amp;amp;px=400" role="button" title="darkblue_0-1715650884753.png" alt="darkblue_0-1715650884753.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, when I use an iPhone, with all other test conditions remaining the same, the genfsk information obtained is as shown in the figure below. At this time, the four KW36 units are unable to obtain the masterRSSI.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="darkblue_1-1715651112719.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/278542iDDA0F904AE40AF96/image-size/medium?v=v2&amp;amp;px=400" role="button" title="darkblue_1-1715651112719.png" alt="darkblue_1-1715651112719.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes I am using&amp;nbsp;&lt;SPAN&gt;connectivity test (GenFSK)&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 01:46:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1864829#M17412</guid>
      <dc:creator>darkblue</dc:creator>
      <dc:date>2024-05-14T01:46:37Z</dc:date>
    </item>
    <item>
      <title>Re: GENFSK can't monitor ios rssi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1865712#M17433</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you in advance for the information proportionate.&lt;/P&gt;
&lt;P&gt;Please let me know if my understanding is correct you have a KW38 with a Heart Rate Sensor example running (with no sleep mode on) and connecting this to your Android phone, while having via CAN 4 KW35 units that are receiving information form the KW38 connection.&lt;/P&gt;
&lt;P&gt;And you have another KW36 that is running the GenFSK connectivity test where you are monitoring the RSSI.&lt;/P&gt;
&lt;P&gt;Please correct me if my understood is incorrect.&lt;/P&gt;
&lt;P&gt;After this said I will like to know the following points:&lt;/P&gt;
&lt;OL type="1"&gt;
&lt;LI value="1"&gt;What is the purpose of this testing?&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;You are looking forward to obtain the RSSI from the peripheral (kw38) or the phone?&lt;/P&gt;
&lt;OL type="1"&gt;
&lt;LI value="2"&gt;Also can you please share with me on a more detailed way how are you running the connectivity test (GenFSK) project.&lt;/LI&gt;
&lt;/OL&gt;
&lt;P&gt;Please let me know this information.&lt;/P&gt;</description>
      <pubDate>Tue, 14 May 2024 21:45:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1865712#M17433</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2024-05-14T21:45:01Z</dc:date>
    </item>
    <item>
      <title>Re: GENFSK can't monitor ios rssi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1865804#M17435</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;SPAN&gt;while having via CAN 4 KW35 units that are receiving information form the KW38 connection.&amp;nbsp;&lt;FONT color="#000000"&gt;&amp;nbsp;Actually,&amp;nbsp; the four monitoring devices are kw36.&amp;nbsp; And yes the four kw36 all running gfsk to get RSSI between cellphone and kw38. In order to accomplish ranging test in vehicle.&amp;nbsp;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;SPAN&gt;&lt;FONT color="#000000"&gt;But It doesn't work when I were using iphone, I've tried iphone 15 pro, iphone 13 etc.&amp;nbsp;&lt;/FONT&gt;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;Also can you please share with me on a more detailed way how are you running the connectivity test (GenFSK) project.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;&lt;SPAN&gt;After I connect my Android phone to the KW38, it conveys parameters such as hopIncrement, crcSeed, syncAddress, connection interval, and channel map to the KW36 device via CAN. Once the XCVR_GENFSK_ENABLED and related features are enabled on the KW36, the GENFSK_InterruptHandler interrupt callback can detect the masterRSSI and slaveRSSI. This process is seamless when I use my Android phone. However, when I switch to an iPhone, the conditional check &lt;/SPAN&gt;if (irqStatus &amp;amp; GENFSK_IRQ_CTRL_RX_IRQ_MASK)&lt;SPAN&gt; doesn't seem to be triggered, suggesting that packets may not be captured. The access address and crcSeed I transmit to the KW36 appear to be correct upon inspection, and there are no obvious anomalies. Could you shed light on what might be causing this issue?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 May 2024 02:06:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1865804#M17435</guid>
      <dc:creator>darkblue</dc:creator>
      <dc:date>2024-05-15T02:06:02Z</dc:date>
    </item>
    <item>
      <title>Re: GENFSK can't monitor ios rssi</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1866592#M17447</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;As y mention on a private message, in order to change the GenFSK to 2M you will have to apply the following changes:&lt;/P&gt;
&lt;UL type="disc"&gt;
&lt;LI&gt;You will need to define the macro for RADIO GEN 3P0 on the fsl_xcvr.h. (image1)&lt;/LI&gt;
&lt;LI&gt;This will enable on the data rate enum to use the 2MBit data rate (image2)&lt;/LI&gt;
&lt;LI&gt;And finally for the change to be applied on the radio configuration change the value to the proper one (image3).&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Please let me know if there is anything else where I can help you.&lt;/P&gt;</description>
      <pubDate>Wed, 15 May 2024 21:50:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/GENFSK-can-t-monitor-ios-rssi/m-p/1866592#M17447</guid>
      <dc:creator>nxf77486</dc:creator>
      <dc:date>2024-05-15T21:50:15Z</dc:date>
    </item>
  </channel>
</rss>