<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN7150 Maximum Output Power in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/PN7150-Maximum-Output-Power/m-p/1831657#M16912</link>
    <description>&lt;P&gt;I have a NFC reader application based on PN7150, currently powered with VBAT=VBAT1=VBAT2=3.3V&lt;BR /&gt;Is the only way to increase output power to increase the VBAT voltage or is there some output Tx setting I could check?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the highest possible output Tx power VBAT=VBAT1=VBAT2=5V, and then update the PMU_CFG register to specify VBAT1=5V and TxLDO = 4.7V ?&lt;/P&gt;</description>
    <pubDate>Wed, 20 Mar 2024 05:27:36 GMT</pubDate>
    <dc:creator>gwctree42</dc:creator>
    <dc:date>2024-03-20T05:27:36Z</dc:date>
    <item>
      <title>PN7150 Maximum Output Power</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN7150-Maximum-Output-Power/m-p/1831657#M16912</link>
      <description>&lt;P&gt;I have a NFC reader application based on PN7150, currently powered with VBAT=VBAT1=VBAT2=3.3V&lt;BR /&gt;Is the only way to increase output power to increase the VBAT voltage or is there some output Tx setting I could check?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is the highest possible output Tx power VBAT=VBAT1=VBAT2=5V, and then update the PMU_CFG register to specify VBAT1=5V and TxLDO = 4.7V ?&lt;/P&gt;</description>
      <pubDate>Wed, 20 Mar 2024 05:27:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN7150-Maximum-Output-Power/m-p/1831657#M16912</guid>
      <dc:creator>gwctree42</dc:creator>
      <dc:date>2024-03-20T05:27:36Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 Maximum Output Power</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN7150-Maximum-Output-Power/m-p/1832255#M16916</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/231190"&gt;@gwctree42&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Please, consider that PN7150 device is not recommended for new designs. We recommend using the&amp;nbsp;&lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-plug-and-play-controller-with-integrated-firmware-and-nci-interface:PN7160" target="_blank"&gt;PN7160&lt;/A&gt; instead.&lt;/P&gt;
&lt;P&gt;TXLDO has the possibility to generate 4.75 V or 4.5 V to supply the transmitter with the regulator being supplied by external 5V. Typical current load should be up to 180mA.&lt;/P&gt;
&lt;P&gt;More information on this can be found in &lt;A href="https://www.nxp.com/docs/en/user-guide/UM10936.pdf" target="_blank"&gt;UM10936&lt;/A&gt;, Section 5.7.2 CFG2 Transmitter supply voltage from external 5V supply; and &lt;A href="https://www.nxp.com/docs/en/data-sheet/PN7150.pdf" target="_blank"&gt;PN7150 Data Sheet&lt;/A&gt;, Section 12.5.3 TXLDO.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Mar 2024 18:25:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN7150-Maximum-Output-Power/m-p/1832255#M16916</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-03-20T18:25:53Z</dc:date>
    </item>
  </channel>
</rss>