<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックPN5190</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/PN5190/m-p/1824605#M16817</link>
    <description>&lt;P&gt;HI Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In one of our design&amp;nbsp; we are using PN5190 chip, as per data sheet it is mentioned that this chip can consume max 2.3W with including internal SW from 3.3V, in this case i have observed in our board the power draw by this chip is 2.6W in that the out put TX line the Power out is like 1 to 1.5W, in this case .&lt;/P&gt;&lt;P&gt;the dropout on chip is 1W or More in this case The thermal issues i am seeing with respective to theoretical and practical also this device is getting&amp;nbsp; more&amp;nbsp; heat. Please help us to under stand more interims of Power consummation, please share if any solution to reduce this .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;/P&gt;&lt;P&gt;Sivaram&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 10 Mar 2024 17:37:10 GMT</pubDate>
    <dc:creator>sivaram1</dc:creator>
    <dc:date>2024-03-10T17:37:10Z</dc:date>
    <item>
      <title>PN5190</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN5190/m-p/1824605#M16817</link>
      <description>&lt;P&gt;HI Team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In one of our design&amp;nbsp; we are using PN5190 chip, as per data sheet it is mentioned that this chip can consume max 2.3W with including internal SW from 3.3V, in this case i have observed in our board the power draw by this chip is 2.6W in that the out put TX line the Power out is like 1 to 1.5W, in this case .&lt;/P&gt;&lt;P&gt;the dropout on chip is 1W or More in this case The thermal issues i am seeing with respective to theoretical and practical also this device is getting&amp;nbsp; more&amp;nbsp; heat. Please help us to under stand more interims of Power consummation, please share if any solution to reduce this .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;/P&gt;&lt;P&gt;Sivaram&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 10 Mar 2024 17:37:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN5190/m-p/1824605#M16817</guid>
      <dc:creator>sivaram1</dc:creator>
      <dc:date>2024-03-10T17:37:10Z</dc:date>
    </item>
    <item>
      <title>Re: PN5190</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN5190/m-p/1833386#M16925</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;PN5190 DPC allows 2 options to reduce the maximum output power:&lt;/P&gt;
&lt;P&gt;1. The target can be reduced.&lt;/P&gt;
&lt;P&gt;2.The maximum VDDPA can be reduced.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to chapter 2 of AN13669 for more details.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Fri, 22 Mar 2024 04:26:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN5190/m-p/1833386#M16925</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2024-03-22T04:26:07Z</dc:date>
    </item>
  </channel>
</rss>