<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic JN5189 chip input pin, how to set the floating input in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-chip-input-pin-how-to-set-the-floating-input/m-p/1821277#M16771</link>
    <description>&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;The pir sensor is connected to the io port of the 5189 as input, which is low when there is no one and high when there is someone. So 5189 io port is set as input, but I want to set floating input(&lt;SPAN&gt;What level is the peripheral device? What level is the IO port&lt;/SPAN&gt;), how to call the function?&lt;/P&gt;&lt;P&gt;I don't set drop-down input. I want to set the float input.How to configure?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomembedded_0-1709625926809.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266492iD9AD5BE0F635D510/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomembedded_0-1709625926809.png" alt="Tomembedded_0-1709625926809.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomembedded_1-1709626222804.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266495i75D6B8C8A60A8D64/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomembedded_1-1709626222804.png" alt="Tomembedded_1-1709626222804.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 05 Mar 2024 08:13:54 GMT</pubDate>
    <dc:creator>Tome-mbedded</dc:creator>
    <dc:date>2024-03-05T08:13:54Z</dc:date>
    <item>
      <title>JN5189 chip input pin, how to set the floating input</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-chip-input-pin-how-to-set-the-floating-input/m-p/1821277#M16771</link>
      <description>&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;The pir sensor is connected to the io port of the 5189 as input, which is low when there is no one and high when there is someone. So 5189 io port is set as input, but I want to set floating input(&lt;SPAN&gt;What level is the peripheral device? What level is the IO port&lt;/SPAN&gt;), how to call the function?&lt;/P&gt;&lt;P&gt;I don't set drop-down input. I want to set the float input.How to configure?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomembedded_0-1709625926809.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266492iD9AD5BE0F635D510/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomembedded_0-1709625926809.png" alt="Tomembedded_0-1709625926809.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Tomembedded_1-1709626222804.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266495i75D6B8C8A60A8D64/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Tomembedded_1-1709626222804.png" alt="Tomembedded_1-1709626222804.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;thank you!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Mar 2024 08:13:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-chip-input-pin-how-to-set-the-floating-input/m-p/1821277#M16771</guid>
      <dc:creator>Tome-mbedded</dc:creator>
      <dc:date>2024-03-05T08:13:54Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 chip input pin, how to set the floating input</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-chip-input-pin-how-to-set-the-floating-input/m-p/1822763#M16800</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/221958"&gt;@Tome-mbedded&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;The following electrical properties are configurable for standard port pins:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;Pull-up/pull-down resistor&lt;/LI&gt;
&lt;LI&gt;Open-drain mode&lt;/LI&gt;
&lt;LI&gt;Inverted function&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;For more information on this, please refer to the &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM11138" target="_blank"&gt;JN5189(T) User manual&lt;/A&gt;, Chapter 12: I/O Pin Configuration (IOCON). Section 12.5 Software control lists some functions and values for IOCON configuration.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Mar 2024 23:20:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-chip-input-pin-how-to-set-the-floating-input/m-p/1822763#M16800</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2024-03-06T23:20:47Z</dc:date>
    </item>
  </channel>
</rss>