<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: PN532 polling</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/PN532-polling/m-p/1813751#M16696</link>
    <description>&lt;P&gt;Thank you Ricardo, as there is no other way to do it rather than sending the command to poll and waiting for response I consider this answered.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;One more question , is NCx3320 and NCx3321 already available on the market? And if so, it is possible to configure them without the&amp;nbsp;NCI interface (I mean normal use of I2C or SPI)?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I'm asking it cause the information about those chips is very limited.&lt;/P&gt;&lt;P&gt;Appreciate your help.&lt;BR /&gt;&lt;BR /&gt;Daniel.&lt;/P&gt;</description>
    <pubDate>Thu, 22 Feb 2024 11:20:43 GMT</pubDate>
    <dc:creator>m3adn</dc:creator>
    <dc:date>2024-02-22T11:20:43Z</dc:date>
    <item>
      <title>PN532 polling</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN532-polling/m-p/1805783#M16649</link>
      <description>&lt;P&gt;Hi.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I have a question regarding &lt;STRONG&gt;PN532&lt;/STRONG&gt;.&lt;BR /&gt;&lt;BR /&gt;Is there any way actually to make PN532 to poll/detect a card (let it be Mifare) without sending commands in loop like&amp;nbsp;&lt;STRONG&gt;InListPassiveTarget&lt;/STRONG&gt;&amp;nbsp;but to receive an interrupt by &lt;STRONG&gt;IRQ&lt;/STRONG&gt; pin whenever there is a card and only then proceed to receive the data?&lt;/P&gt;&lt;P&gt;I found that that later versions such as&amp;nbsp;&lt;SPAN&gt;&lt;STRONG&gt;PN7120&lt;/STRONG&gt; / &lt;STRONG&gt;PN7150&lt;/STRONG&gt;&amp;nbsp;support&amp;nbsp;&lt;STRONG&gt;LPCD&lt;/STRONG&gt;, which I think fits my requirements, but I'd need a confirmation to the fact that in order to retrieve&amp;nbsp;any data from the card I should send a command and only then read the card.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I found this topic&amp;nbsp;&lt;A title="another topic about it" href="https://community.nxp.com/t5/NFC/How-to-generate-an-interrupt-to-the-processor-when-a-tag-is/m-p/589066" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/NFC/How-to-generate-an-interrupt-to-the-processor-when-a-tag-is/m-p/589066&lt;/A&gt;&amp;nbsp;talking about similar.&lt;BR /&gt;&lt;BR /&gt;Any help is appreciated.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Ty.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Feb 2024 12:00:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN532-polling/m-p/1805783#M16649</guid>
      <dc:creator>m3adn</dc:creator>
      <dc:date>2024-02-13T12:00:47Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 polling</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN532-polling/m-p/1806061#M16652</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. First of all, PN532 is a product that is not recommended for new designs.&lt;/P&gt;
&lt;P&gt;I would recommend checking this &lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN133910.pdf" target="_blank"&gt;Application Note&lt;/A&gt;. Please refer to section 3.3.&lt;/P&gt;
&lt;P&gt;Also, I would recommend checking our &lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/nfc-plug-and-play-controller-with-integrated-firmware-and-nci-interface:PN7160" target="_blank"&gt;PN7160 | NFC Controller with Integrated Firmware and NCI Interface.&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Tue, 13 Feb 2024 18:27:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN532-polling/m-p/1806061#M16652</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2024-02-13T18:27:25Z</dc:date>
    </item>
    <item>
      <title>Re: PN532 polling</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN532-polling/m-p/1813751#M16696</link>
      <description>&lt;P&gt;Thank you Ricardo, as there is no other way to do it rather than sending the command to poll and waiting for response I consider this answered.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;One more question , is NCx3320 and NCx3321 already available on the market? And if so, it is possible to configure them without the&amp;nbsp;NCI interface (I mean normal use of I2C or SPI)?&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I'm asking it cause the information about those chips is very limited.&lt;/P&gt;&lt;P&gt;Appreciate your help.&lt;BR /&gt;&lt;BR /&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Feb 2024 11:20:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN532-polling/m-p/1813751#M16696</guid>
      <dc:creator>m3adn</dc:creator>
      <dc:date>2024-02-22T11:20:43Z</dc:date>
    </item>
  </channel>
</rss>