<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic VLAN Configuration SJA1105Q in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/VLAN-Configuration-SJA1105Q/m-p/1809620#M16665</link>
    <description>&lt;P&gt;Hi, I am looking through the data sheets, application hints, and software user manual for the&amp;nbsp;SJA1105Q automotive ethernet IC. Looking through the example python scripts for the&amp;nbsp;SJA1105Q development board&amp;nbsp;AH1707, I am confused by the write_vlan_lookup_table.py file. I am confused by the hex values used for VMEMB_PORT and all of the following hex values for the configuration variables. Why are the member ports set to 0x07? My understanding has been to convert it to binary (0b00111) which corresponds to ports 0, 1, and 2 (or 3 and 4) being set as the member ports for this VLAN. The comment next to this line of code states&amp;nbsp;##Member ports (_ _ _ P4 P3 P2 P1 P0) which I don't understand either.&lt;/P&gt;&lt;P&gt;The intended use case for me is to have 3 VLANs where&lt;/P&gt;&lt;P&gt;P0 &amp;lt;--&amp;gt; P1 VLAN 0&lt;BR /&gt;P0 &amp;lt;--&amp;gt; P2 VLAN 1&lt;/P&gt;&lt;P&gt;P0 &amp;lt;--&amp;gt; P3 VLAN 2&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated!&lt;/P&gt;</description>
    <pubDate>Thu, 15 Feb 2024 22:59:51 GMT</pubDate>
    <dc:creator>scallaway</dc:creator>
    <dc:date>2024-02-15T22:59:51Z</dc:date>
    <item>
      <title>VLAN Configuration SJA1105Q</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/VLAN-Configuration-SJA1105Q/m-p/1809620#M16665</link>
      <description>&lt;P&gt;Hi, I am looking through the data sheets, application hints, and software user manual for the&amp;nbsp;SJA1105Q automotive ethernet IC. Looking through the example python scripts for the&amp;nbsp;SJA1105Q development board&amp;nbsp;AH1707, I am confused by the write_vlan_lookup_table.py file. I am confused by the hex values used for VMEMB_PORT and all of the following hex values for the configuration variables. Why are the member ports set to 0x07? My understanding has been to convert it to binary (0b00111) which corresponds to ports 0, 1, and 2 (or 3 and 4) being set as the member ports for this VLAN. The comment next to this line of code states&amp;nbsp;##Member ports (_ _ _ P4 P3 P2 P1 P0) which I don't understand either.&lt;/P&gt;&lt;P&gt;The intended use case for me is to have 3 VLANs where&lt;/P&gt;&lt;P&gt;P0 &amp;lt;--&amp;gt; P1 VLAN 0&lt;BR /&gt;P0 &amp;lt;--&amp;gt; P2 VLAN 1&lt;/P&gt;&lt;P&gt;P0 &amp;lt;--&amp;gt; P3 VLAN 2&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated!&lt;/P&gt;</description>
      <pubDate>Thu, 15 Feb 2024 22:59:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/VLAN-Configuration-SJA1105Q/m-p/1809620#M16665</guid>
      <dc:creator>scallaway</dc:creator>
      <dc:date>2024-02-15T22:59:51Z</dc:date>
    </item>
    <item>
      <title>Re: VLAN Configuration SJA1105Q</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/VLAN-Configuration-SJA1105Q/m-p/1810607#M16672</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229590"&gt;@scallaway&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;the comment "##Member ports (_ _ _ P4 P3 P2 P1 P0)" shows the bit mapping. &lt;BR /&gt;P0 corresponds to 0x01, P1 corresponds to 0x02 etc. Upper three bits are not used because there are 5 ports only. &lt;BR /&gt;I agree that this is not very clear in the documentation. &lt;BR /&gt;I found this example in AH1704 which explains it a bit:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="lukaszadrapa_0-1708324832787.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263639i1F391D8BEAB019B8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="lukaszadrapa_0-1708324832787.png" alt="lukaszadrapa_0-1708324832787.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;lukaszadrapa_0-1708324832787.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Lukas&lt;/P&gt;</description>
      <pubDate>Mon, 19 Feb 2024 06:42:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/VLAN-Configuration-SJA1105Q/m-p/1810607#M16672</guid>
      <dc:creator>lukaszadrapa</dc:creator>
      <dc:date>2024-02-19T06:42:53Z</dc:date>
    </item>
    <item>
      <title>Re: VLAN Configuration SJA1105Q</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/VLAN-Configuration-SJA1105Q/m-p/1811085#M16674</link>
      <description>Thank you, Lukas!</description>
      <pubDate>Mon, 19 Feb 2024 17:00:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/VLAN-Configuration-SJA1105Q/m-p/1811085#M16674</guid>
      <dc:creator>scallaway</dc:creator>
      <dc:date>2024-02-19T17:00:20Z</dc:date>
    </item>
  </channel>
</rss>