<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ***JLink Error: Could not start CPU core. (ErrorCode: -2) in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JLink-Error-Could-not-start-CPU-core-ErrorCode-2/m-p/1797595#M16551</link>
    <description>&lt;P&gt;same error message.&lt;/P&gt;&lt;P&gt;Any solution on this?&lt;/P&gt;</description>
    <pubDate>Tue, 30 Jan 2024 08:41:34 GMT</pubDate>
    <dc:creator>Ekta01</dc:creator>
    <dc:date>2024-01-30T08:41:34Z</dc:date>
    <item>
      <title>***JLink Error: Could not start CPU core. (ErrorCode: -2)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JLink-Error-Could-not-start-CPU-core-ErrorCode-2/m-p/847067#M5721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Target info:&lt;BR /&gt;------------&lt;BR /&gt;Device: QN9080C&lt;BR /&gt;VTarget = 3.300V&lt;BR /&gt;State of Pins: &lt;BR /&gt;TCK: 0, TDI: 0, TDO: 1, TMS: 0, TRES: 1, TRST: 1&lt;BR /&gt;Hardware-Breakpoints: 6&lt;BR /&gt;Software-Breakpoints: 8192&lt;BR /&gt;Watchpoints: 4&lt;BR /&gt;JTAG speed: 200 kHz&lt;BR /&gt; &lt;BR /&gt;***JLink Error: Could not start CPU core. (ErrorCode: -2)&lt;BR /&gt;***JLink Error: Can not read register 15 (R15) while CPU is running&lt;BR /&gt;***JLink Error: Can not read register 20 (CFBP) while CPU is running&lt;BR /&gt;***JLink Error: CPU is not halted&lt;BR /&gt;***JLink Error: Can not read register 15 (R15) while CPU is running&lt;BR /&gt;Full Chip Erase Failed!&lt;BR /&gt;Error: Flash Download failed - "Cortex-M4"&lt;BR /&gt;Flash Load finished at 12:18:04&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;使用开发板可以正常烧些。电路部分检查也没有问题. pin33管脚（chip_mode) 如果接GND，SWD 就找不到核心了。&lt;/P&gt;&lt;P&gt;不知道问题&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Aug 2018 04:23:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JLink-Error-Could-not-start-CPU-core-ErrorCode-2/m-p/847067#M5721</guid>
      <dc:creator>wuhanpin</dc:creator>
      <dc:date>2018-08-31T04:23:44Z</dc:date>
    </item>
    <item>
      <title>Re: ***JLink Error: Could not start CPU core. (ErrorCode: -2)</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JLink-Error-Could-not-start-CPU-core-ErrorCode-2/m-p/1797595#M16551</link>
      <description>&lt;P&gt;same error message.&lt;/P&gt;&lt;P&gt;Any solution on this?&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jan 2024 08:41:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JLink-Error-Could-not-start-CPU-core-ErrorCode-2/m-p/1797595#M16551</guid>
      <dc:creator>Ekta01</dc:creator>
      <dc:date>2024-01-30T08:41:34Z</dc:date>
    </item>
  </channel>
</rss>