<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: JN5189</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5189/m-p/1789918#M16442</link>
    <description>&lt;P&gt;HI,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/21716"&gt;@wenbaoli&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;请问您使用的SDK版本是多少？&lt;/P&gt;&lt;P&gt;您用的是哪个example？&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards，&lt;/P&gt;&lt;P&gt;Christine.&lt;/P&gt;</description>
    <pubDate>Wed, 17 Jan 2024 03:30:58 GMT</pubDate>
    <dc:creator>Christine_Li</dc:creator>
    <dc:date>2024-01-17T03:30:58Z</dc:date>
    <item>
      <title>JN5189</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189/m-p/1788356#M16416</link>
      <description>&lt;P&gt;我启动MMAC功能后，打开中断后，发送数据后一直进入中断处理函数，而且不能进入回调函数；&lt;/P&gt;&lt;P&gt;我没有办法找到清除中断标志的方法，请帮我解决这个问题，谢谢。&lt;/P&gt;&lt;P&gt;以下是代码：&lt;/P&gt;&lt;P&gt;vRadio_ActivateXtal32MRadioBiasing();&lt;BR /&gt;vRadio_Temp_Update(40);&lt;BR /&gt;&lt;BR /&gt;vMMAC_Enable();&lt;BR /&gt;vMMAC_ConfigureRadio();&lt;BR /&gt;vMMAC_EnableInterrupts(MAC_IRQHandler_Callback);&lt;BR /&gt;// vMMAC_ConfigureInterruptSources(E_MMAC_INT_TX_COMPLETE | E_MMAC_INT_RX_COMPLETE); //ENABLE_RAM_VECTOR_TABLE=1&lt;BR /&gt;// vMMAC_SetChannelAndPower(11, i8MMAC_GetTxPowerLevel());&lt;BR /&gt;&lt;BR /&gt;// vMMAC_EnableAntennaDiversity();&lt;BR /&gt;// vMMAC_SetTxParameters();&lt;BR /&gt;&lt;BR /&gt;TxMacFrame.u8PayloadLength = sizeof("MMAC_Transmit_Test");&lt;BR /&gt;TxMacFrame.u8SequenceNum = 1;&lt;BR /&gt;TxMacFrame.u16FCF = 0;&lt;BR /&gt;TxMacFrame.u16DestPAN = 1;&lt;BR /&gt;TxMacFrame.u16SrcPAN = 1;&lt;BR /&gt;TxMacFrame.uDestAddr.u16Short = 2;&lt;BR /&gt;TxMacFrame.uSrcAddr.u16Short = 1;&lt;BR /&gt;TxMacFrame.u16FCS = 0;&lt;BR /&gt;memcpy(TxMacFrame.uPayload.au8Byte, "MMAC_Transmit_Test", sizeof("MMAC_Transmit_Test"));&lt;BR /&gt;TxOption = E_MMAC_TX_START_NOW | E_MMAC_TX_NO_AUTO_ACK | E_MMAC_TX_NO_CCA;&lt;BR /&gt;&lt;BR /&gt;for (;;)&lt;BR /&gt;{&lt;BR /&gt;if (++time_cnt &amp;gt;= 50)&lt;BR /&gt;{&lt;BR /&gt;time_cnt = 0;&lt;BR /&gt;&lt;BR /&gt;vMMAC_StartMacTransmit(&amp;amp;TxMacFrame, (teTxOption)TxOption);&lt;BR /&gt;&lt;BR /&gt;evnt_Cnt++;&lt;BR /&gt;PRINTF("Default Task vMMAC MacTransmit cnt: %d.\r\n", evnt_Cnt);&lt;BR /&gt;}&lt;BR /&gt;&lt;BR /&gt;vTaskDelay(10);&lt;BR /&gt;}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;void MAC_IRQHandler_Callback (uint32 u32InterruptBitmap)&lt;BR /&gt;{&lt;BR /&gt;/* Is the interrupt for Transmit completed */&lt;BR /&gt;if (u32InterruptBitmap &amp;amp; E_MMAC_INT_TX_COMPLETE)&lt;BR /&gt;{&lt;BR /&gt;bTxComplete = TRUE;&lt;BR /&gt;}&lt;BR /&gt;/* Is the interrupt for Rx completed */&lt;BR /&gt;else if((u32InterruptBitmap &amp;amp; E_MMAC_INT_RX_COMPLETE))&lt;BR /&gt;{&lt;BR /&gt;bRxComplete = TRUE;&lt;BR /&gt;}&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;//打开中断后只能运行一次vMMAC_StartMacTransmit，然后就是无休止的进入以下中断&lt;/P&gt;&lt;P&gt;void ZIGBEE_MAC_IRQHandler (void)&amp;nbsp;&amp;nbsp;&lt;BR /&gt;{&lt;BR /&gt;NVIC_ClearPendingIRQ(ZIGBEE_MAC_IRQn);&lt;BR /&gt;// NVIC_DisableIRQ(ZIGBEE_MAC_IRQn);&lt;BR /&gt;}&lt;/P&gt;</description>
      <pubDate>Sun, 14 Jan 2024 10:49:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189/m-p/1788356#M16416</guid>
      <dc:creator>wenbaoli</dc:creator>
      <dc:date>2024-01-14T10:49:12Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189/m-p/1789431#M16435</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/21716"&gt;@wenbaoli&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I will check it in my local side, and reply to you ASAP.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Christine.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Jan 2024 10:30:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189/m-p/1789431#M16435</guid>
      <dc:creator>Christine_Li</dc:creator>
      <dc:date>2024-01-16T10:30:40Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189/m-p/1789918#M16442</link>
      <description>&lt;P&gt;HI,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/21716"&gt;@wenbaoli&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;请问您使用的SDK版本是多少？&lt;/P&gt;&lt;P&gt;您用的是哪个example？&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards，&lt;/P&gt;&lt;P&gt;Christine.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jan 2024 03:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189/m-p/1789918#M16442</guid>
      <dc:creator>Christine_Li</dc:creator>
      <dc:date>2024-01-17T03:30:58Z</dc:date>
    </item>
  </channel>
</rss>