<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックBluetooth Low Energy v4.1 Role Switching</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Bluetooth-Low-Energy-v4-1-Role-Switching/m-p/359501#M164</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One of the key enhancements for BLE in v4.1 is the added support for a slave device to be able to connect to &lt;STRONG&gt;TWO&lt;/STRONG&gt; master devices, i.e., the slave device can simultaneously belong to two star networks. This was not allowed in v4.0 specification.&lt;/P&gt;&lt;P&gt;A slave device can also act as a bridge between two star networks. However, this is not explicitly covered in v4.1 of the spec. The topic of a slave devices to act as a bridge between two star networks and the master-slave role-switching are expected to be resolved in future versions of the specification.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Sep 2014 23:13:15 GMT</pubDate>
    <dc:creator>kelvinleung</dc:creator>
    <dc:date>2014-09-30T23:13:15Z</dc:date>
    <item>
      <title>Bluetooth Low Energy v4.1 Role Switching</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Bluetooth-Low-Energy-v4-1-Role-Switching/m-p/359501#M164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One of the key enhancements for BLE in v4.1 is the added support for a slave device to be able to connect to &lt;STRONG&gt;TWO&lt;/STRONG&gt; master devices, i.e., the slave device can simultaneously belong to two star networks. This was not allowed in v4.0 specification.&lt;/P&gt;&lt;P&gt;A slave device can also act as a bridge between two star networks. However, this is not explicitly covered in v4.1 of the spec. The topic of a slave devices to act as a bridge between two star networks and the master-slave role-switching are expected to be resolved in future versions of the specification.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Sep 2014 23:13:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Bluetooth-Low-Energy-v4-1-Role-Switching/m-p/359501#M164</guid>
      <dc:creator>kelvinleung</dc:creator>
      <dc:date>2014-09-30T23:13:15Z</dc:date>
    </item>
  </channel>
</rss>