<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックHow to return to ota_client or how to reload code through ota with KW38?</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/How-to-return-to-ota-client-or-how-to-reload-code-through-ota/m-p/1787525#M16397</link>
    <description>&lt;P&gt;hello&lt;BR /&gt;I am using the KW38 bluethoot module&lt;BR /&gt;use the example codes _bootloader_ota and ota_client_att&lt;BR /&gt;and the glucose_sensor_bm example&lt;BR /&gt;I followed the steps mentioned in this link&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/KW38-Reprogramming-a-KW38-device-using-the-OTAP-Client-Software/ta-p/1169834" target="_blank"&gt;https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/KW38-Reprogramming-a-KW38-device-using-the-OTAP-Client-Software/ta-p/1169834&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;everything works well&lt;BR /&gt;but now I want to know how to return the stack of the ota_client code example? to load any code through ota several times&lt;/P&gt;&lt;P&gt;I don't want to start the first steps mentioned in that link... I want to reload code through ota after loading&amp;nbsp;the glucose_sensor_bm or wireless_uart&amp;nbsp;codes examples, or any code but not in a wired way&lt;/P&gt;</description>
    <pubDate>Thu, 11 Jan 2024 23:03:09 GMT</pubDate>
    <dc:creator>Ingm</dc:creator>
    <dc:date>2024-01-11T23:03:09Z</dc:date>
    <item>
      <title>How to return to ota_client or how to reload code through ota with KW38?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/How-to-return-to-ota-client-or-how-to-reload-code-through-ota/m-p/1787525#M16397</link>
      <description>&lt;P&gt;hello&lt;BR /&gt;I am using the KW38 bluethoot module&lt;BR /&gt;use the example codes _bootloader_ota and ota_client_att&lt;BR /&gt;and the glucose_sensor_bm example&lt;BR /&gt;I followed the steps mentioned in this link&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/KW38-Reprogramming-a-KW38-device-using-the-OTAP-Client-Software/ta-p/1169834" target="_blank"&gt;https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/KW38-Reprogramming-a-KW38-device-using-the-OTAP-Client-Software/ta-p/1169834&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;everything works well&lt;BR /&gt;but now I want to know how to return the stack of the ota_client code example? to load any code through ota several times&lt;/P&gt;&lt;P&gt;I don't want to start the first steps mentioned in that link... I want to reload code through ota after loading&amp;nbsp;the glucose_sensor_bm or wireless_uart&amp;nbsp;codes examples, or any code but not in a wired way&lt;/P&gt;</description>
      <pubDate>Thu, 11 Jan 2024 23:03:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/How-to-return-to-ota-client-or-how-to-reload-code-through-ota/m-p/1787525#M16397</guid>
      <dc:creator>Ingm</dc:creator>
      <dc:date>2024-01-11T23:03:09Z</dc:date>
    </item>
    <item>
      <title>Re: How to return to ota_client or how to reload code through ota with KW38?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/How-to-return-to-ota-client-or-how-to-reload-code-through-ota/m-p/1788129#M16412</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;I would recommend you checking this Application Note: &lt;A href="https://www.nxp.com/docs/en/application-note/AN12979.pdf" target="_blank"&gt;KW38 - Integrating the OTAP Client Service into a Bluetooth LE Peripheral Device Application Note (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;You would need to implement some changes on the SDK example, to integrate OTAP feature.&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Fri, 12 Jan 2024 16:15:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/How-to-return-to-ota-client-or-how-to-reload-code-through-ota/m-p/1788129#M16412</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2024-01-12T16:15:13Z</dc:date>
    </item>
  </channel>
</rss>