<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: connect PX533 using libnfc in python</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1781807#M16319</link>
    <description>&lt;P&gt;I will contact them but am also open to sign an NDA and test the software as well. Thanks for your help.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 02 Jan 2024 18:57:45 GMT</pubDate>
    <dc:creator>bartmuskala</dc:creator>
    <dc:date>2024-01-02T18:57:45Z</dc:date>
    <item>
      <title>connect PX533 using libnfc in python</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1781747#M16316</link>
      <description>&lt;P&gt;I have ordered a DL533N reader based on the NXP PR533 chip.&lt;/P&gt;&lt;P&gt;I have installed all required libraries. I try to find the NFC reader on my raspberry Pi 400. No luck...&lt;/P&gt;&lt;P&gt;I keep getting a "No NFC device found" on nfc-list.&lt;BR /&gt;Using pn53x-tamashell I get "pn53x-tamashell: ERROR: Unable to open NFC device."&lt;/P&gt;&lt;P&gt;I don't know where to start honestly. Have been googling, chat gpting and the likes.&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 15:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1781747#M16316</guid>
      <dc:creator>bartmuskala</dc:creator>
      <dc:date>2024-01-02T15:15:40Z</dc:date>
    </item>
    <item>
      <title>Re: connect PX533 using libnfc in python</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1781805#M16318</link>
      <description>&lt;P lang="es-MX"&gt;Hello sir,&lt;/P&gt;
&lt;P lang="es-MX"&gt;My recommendation is that please contact Digital Logic for further information since, &lt;A href="https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/usb-nfc-integrated-reader-solution:PR5331C3HN" target="_blank"&gt;PR533&lt;/A&gt; is a USB-integrated solution but, the direct support for LibNFC inst directly supported by us. Is possible that the version of LibNFC you are using, requires some adjustments to the shell script provided by d-logic.&lt;/P&gt;
&lt;P lang="es-MX"&gt;In case you are interested in testing the PR533, we do provide a product support package but, it requires you to sign an NDA with NXP for access to downloading it.&lt;/P&gt;
&lt;P lang="es-MX"&gt;Still, I can't assure you that our provided software will fully work with the DL533N directly since, I'm not fully sure how it is built.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 18:53:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1781805#M16318</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2024-01-02T18:53:57Z</dc:date>
    </item>
    <item>
      <title>Re: connect PX533 using libnfc in python</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1781807#M16319</link>
      <description>&lt;P&gt;I will contact them but am also open to sign an NDA and test the software as well. Thanks for your help.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 18:57:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1781807#M16319</guid>
      <dc:creator>bartmuskala</dc:creator>
      <dc:date>2024-01-02T18:57:45Z</dc:date>
    </item>
    <item>
      <title>Re: connect PX533 using libnfc in python</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1781837#M16321</link>
      <description>&lt;P&gt;Re-reading your remark, I was wondering whether there was another method to connect using Python on raspberry Pi? Libnfc was the option I believed to use, but if there are other options that you can provide this is also good. I need it to connect and to read data from the card. Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 21:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1781837#M16321</guid>
      <dc:creator>bartmuskala</dc:creator>
      <dc:date>2024-01-02T21:33:17Z</dc:date>
    </item>
    <item>
      <title>Re: connect PX533 using libnfc in python</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1782475#M16329</link>
      <description>&lt;P lang="es-MX"&gt;Hello sir,&lt;/P&gt;
&lt;P lang="es-MX"&gt;Unfortunately, we don't have any tool for Linux or based in Python that I can recommend. Although, you can use a PCSC tool that may suit your needs. Since the PR553 is a USB solution, the NXP IC should be able to interface through these commands.&lt;/P&gt;
&lt;P lang="es-MX"&gt;Regarding the interest in signing an NDA, please take a look at the following FAQs: &lt;A href="https://www.nxp.com/support/support/non-disclosure-agreement-faqs:NDA-FAQS" target="_blank"&gt;https://www.nxp.com/support/support/non-disclosure-agreement-faqs:NDA-FAQS&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 03 Jan 2024 20:20:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/connect-PX533-using-libnfc-in-python/m-p/1782475#M16329</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2024-01-03T20:20:38Z</dc:date>
    </item>
  </channel>
</rss>