<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックPerform secured firmware update for PN5190 using NFC Cockpit GUI</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Perform-secured-firmware-update-for-PN5190-using-NFC-Cockpit-GUI/m-p/1772769#M16168</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm working on an NFC application that uses PN5190 and&amp;nbsp;IMX 7 as a Host uC. I want to use the Secure Firmware Update feature provided by the GUI to upgrade the firmware for PN5190.&lt;/P&gt;&lt;P&gt;The feature works perfectly on the PNEV5190B dev kit which has K82 as a Host uC. Ideally, I want to find the UcBalFW used for the K82 in the dev kit and port it to IMX 7. However, it seems the latest UCBalFW source code supporting PN5190 (NxpNfcCockpit_VCOM_UcBalFW_v03.09.00) doesn't support/provide interfaces for the Secure Firmware Update.&lt;/P&gt;&lt;P&gt;Do you have or know where to find an example source code that I need?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tuan&lt;/P&gt;</description>
    <pubDate>Tue, 12 Dec 2023 05:10:28 GMT</pubDate>
    <dc:creator>tuanbui</dc:creator>
    <dc:date>2023-12-12T05:10:28Z</dc:date>
    <item>
      <title>Perform secured firmware update for PN5190 using NFC Cockpit GUI</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Perform-secured-firmware-update-for-PN5190-using-NFC-Cockpit-GUI/m-p/1772769#M16168</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm working on an NFC application that uses PN5190 and&amp;nbsp;IMX 7 as a Host uC. I want to use the Secure Firmware Update feature provided by the GUI to upgrade the firmware for PN5190.&lt;/P&gt;&lt;P&gt;The feature works perfectly on the PNEV5190B dev kit which has K82 as a Host uC. Ideally, I want to find the UcBalFW used for the K82 in the dev kit and port it to IMX 7. However, it seems the latest UCBalFW source code supporting PN5190 (NxpNfcCockpit_VCOM_UcBalFW_v03.09.00) doesn't support/provide interfaces for the Secure Firmware Update.&lt;/P&gt;&lt;P&gt;Do you have or know where to find an example source code that I need?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Tuan&lt;/P&gt;</description>
      <pubDate>Tue, 12 Dec 2023 05:10:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Perform-secured-firmware-update-for-PN5190-using-NFC-Cockpit-GUI/m-p/1772769#M16168</guid>
      <dc:creator>tuanbui</dc:creator>
      <dc:date>2023-12-12T05:10:28Z</dc:date>
    </item>
    <item>
      <title>Re: Perform secured firmware update for PN5190 using NFC Cockpit GUI</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Perform-secured-firmware-update-for-PN5190-using-NFC-Cockpit-GUI/m-p/1773436#M16180</link>
      <description>&lt;P&gt;Hello, my name is Fabian, I've been assigned to support your case.&lt;/P&gt;
&lt;P&gt;I appreciate your interest in our products.&lt;/P&gt;
&lt;P&gt;Could you please let me know which MPU are you using?&lt;/P&gt;
&lt;P&gt;I have to check internally how can we proceed with the porting of the FW project based on the MPU.&lt;/P&gt;</description>
      <pubDate>Tue, 12 Dec 2023 23:59:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Perform-secured-firmware-update-for-PN5190-using-NFC-Cockpit-GUI/m-p/1773436#M16180</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2023-12-12T23:59:00Z</dc:date>
    </item>
    <item>
      <title>Re: Perform secured firmware update for PN5190 using NFC Cockpit GUI</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Perform-secured-firmware-update-for-PN5190-using-NFC-Cockpit-GUI/m-p/1775137#M16207</link>
      <description>&lt;P&gt;Hi Fabian,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;I recently found the problem is due to a permission issue which prevents the IMX 7 from toggling the EN pin of PN5190. As a result, the PN5190 failed to enter download mode.&amp;nbsp;&lt;/P&gt;&lt;P&gt;After adjusting the permission, use the UcBalFW provided (v3.09.00)&amp;nbsp; the secured downloading seems to work correctly.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tuan&lt;/P&gt;</description>
      <pubDate>Thu, 14 Dec 2023 22:31:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Perform-secured-firmware-update-for-PN5190-using-NFC-Cockpit-GUI/m-p/1775137#M16207</guid>
      <dc:creator>tuanbui</dc:creator>
      <dc:date>2023-12-14T22:31:48Z</dc:date>
    </item>
  </channel>
</rss>