<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: PN5180: Timer1 not run</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1761657#M16008</link>
    <description>&lt;P&gt;could you please let me know how can I reproduce this issue on my side with PN5180 EVK board?&amp;nbsp; For the MCU timer, and timer on PN5180,&amp;nbsp; maybe the difference is the accuracy.&amp;nbsp; &amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can set a bit in the ISR of Timer1, to check whether Timer1 is run.&lt;/P&gt;</description>
    <pubDate>Wed, 22 Nov 2023 07:16:29 GMT</pubDate>
    <dc:creator>danielchen</dc:creator>
    <dc:date>2023-11-22T07:16:29Z</dc:date>
    <item>
      <title>PN5180: Timer1 not run</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1754887#M15878</link>
      <description>&lt;P&gt;Hi NXP technical team,&lt;/P&gt;&lt;P&gt;I am using custom PN5180 board base on your PN5180 schenematic but sometimes when I send REQA command (ISO14443A-3) without the card, the function&amp;nbsp;phhalHw_Pn5180_WaitIrq run infinity (not using PN5180_IRQ pin).&lt;BR /&gt;&lt;BR /&gt;I check it and i found this in pnhalHw_Pn5180_Wait.c :&lt;BR /&gt;do&lt;BR /&gt;{&lt;BR /&gt;/* Read the IRQ register and check if the interrupt has occured */&lt;BR /&gt;PH_CHECK_SUCCESS_FCT(statusTmp, phhalHw_Pn5180_Instr_ReadRegister(pDataParams, IRQ_STATUS, &amp;amp;dwRegister));&lt;BR /&gt;}while(!(dwRegister &amp;amp; dwIrqWaitFor));&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;I tried read TIMER1_STATUS register during the while statement but T1_VALUE field not change while T1_RUNNING field = 1.&lt;/P&gt;&lt;P&gt;What causes this problem?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 09 Nov 2023 10:24:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1754887#M15878</guid>
      <dc:creator>TrungDT</dc:creator>
      <dc:date>2023-11-09T10:24:59Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180: Timer1 not run</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1759833#M15975</link>
      <description>&lt;P&gt;If you put one tag in the range of the antenna the application should ends the loop and move on.&lt;/P&gt;</description>
      <pubDate>Mon, 20 Nov 2023 11:34:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1759833#M15975</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2023-11-20T11:34:23Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180: Timer1 not run</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1760181#M15977</link>
      <description>&lt;P&gt;Hi danielchen,&lt;BR /&gt;&lt;BR /&gt;Thanks for your answer.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;I also made a new one, and sometimes it still goes into the infinity loop. As your answer, the new one ends the loop when I put the tag in the range of its antenna, but the old one cannot.&lt;BR /&gt;&lt;BR /&gt;Can I ask what the reason causes this problem? Can I fix it with either software or hardware or both?&lt;BR /&gt;&lt;BR /&gt;I am temporarily fixing this problem using the MCU timer with the given timeout value, which is the same as the PN5180 Timer1 timeout value.&lt;BR /&gt;&lt;BR /&gt;Thanks and best regards.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Nov 2023 01:28:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1760181#M15977</guid>
      <dc:creator>TrungDT</dc:creator>
      <dc:date>2023-11-21T01:28:34Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180: Timer1 not run</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1761657#M16008</link>
      <description>&lt;P&gt;could you please let me know how can I reproduce this issue on my side with PN5180 EVK board?&amp;nbsp; For the MCU timer, and timer on PN5180,&amp;nbsp; maybe the difference is the accuracy.&amp;nbsp; &amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can set a bit in the ISR of Timer1, to check whether Timer1 is run.&lt;/P&gt;</description>
      <pubDate>Wed, 22 Nov 2023 07:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1761657#M16008</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2023-11-22T07:16:29Z</dc:date>
    </item>
    <item>
      <title>Re: PN5180: Timer1 not run</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1762415#M16013</link>
      <description>&lt;P&gt;I polling the tag by sending REQA command&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;frequently in loop of main&amp;nbsp; and sometime the system run into crashes.&lt;/P&gt;&lt;P&gt;I am using&amp;nbsp;&lt;SPAN&gt;phpalI14443p3a_Sw_RequestA function for sending REQA command.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When the system is crashed, I still check the TIMER1_STATUS register, the T1_RUNNING field (bit 20) adrealy set to 1 but the T1_VALUE field not change.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I am worried the the cause of the error is our hardware. I think the issue due to passive electronic components error (do not meet reference).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 23 Nov 2023 07:11:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN5180-Timer1-not-run/m-p/1762415#M16013</guid>
      <dc:creator>TrungDT</dc:creator>
      <dc:date>2023-11-23T07:11:05Z</dc:date>
    </item>
  </channel>
</rss>