<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックMMZ09332BT1</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1/m-p/1728913#M15713</link>
    <description>&lt;P&gt;&lt;SPAN&gt;I want to use the MMZ09332BT1 in the frequency range 760-870 MHz, but with FR4 instead of RO4350B. I will change the trace width in the RF out and RF lines to achieve an impedance of 50 ohms. Should I consider anything else, such as the length of the VCC line?If the component was perfectly internally matched, I would make this change (using FR4) with confidence. However, the MMZ09332BT1 data sheet says that it "requires minimal external matching."&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 25 Sep 2023 12:06:01 GMT</pubDate>
    <dc:creator>bsky2345</dc:creator>
    <dc:date>2023-09-25T12:06:01Z</dc:date>
    <item>
      <title>MMZ09332BT1</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1/m-p/1728913#M15713</link>
      <description>&lt;P&gt;&lt;SPAN&gt;I want to use the MMZ09332BT1 in the frequency range 760-870 MHz, but with FR4 instead of RO4350B. I will change the trace width in the RF out and RF lines to achieve an impedance of 50 ohms. Should I consider anything else, such as the length of the VCC line?If the component was perfectly internally matched, I would make this change (using FR4) with confidence. However, the MMZ09332BT1 data sheet says that it "requires minimal external matching."&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 12:06:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1/m-p/1728913#M15713</guid>
      <dc:creator>bsky2345</dc:creator>
      <dc:date>2023-09-25T12:06:01Z</dc:date>
    </item>
    <item>
      <title>Re: MMZ09332BT1</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1/m-p/1729155#M15718</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Substrate dielectric permittivity and thickness is critical. The width input/output traces is set to provide 50 Ohm impedance.&lt;/P&gt;&lt;P&gt;Datasheet specifies substrate RO4350B, Dk=3.66, the thickness is 10mil top dielectric layer. Three dielectric layers with total thickness of 32 mils.&lt;/P&gt;&lt;P&gt;Typical FR-4 has Dk=4.8. You can use the same layout as in the datasheet but the top dielectric layer thickness should be 12.3 mils (small variations possible, 12mils).&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 21:33:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1/m-p/1729155#M15718</guid>
      <dc:creator>ErikaC</dc:creator>
      <dc:date>2023-09-25T21:33:25Z</dc:date>
    </item>
    <item>
      <title>Re: MMZ09332BT1</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1/m-p/1733178#M15738</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;This tips help me and I redesign my pcb and sent for production.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Tue, 03 Oct 2023 13:58:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1/m-p/1733178#M15738</guid>
      <dc:creator>bsky2345</dc:creator>
      <dc:date>2023-10-03T13:58:02Z</dc:date>
    </item>
  </channel>
</rss>