<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: FRDM-KW38 FSCI using I2C</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW38-FSCI-using-I2C/m-p/1707053#M15483</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219236"&gt;@Ajay1202&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can use the ble_fsci_black_box (inside wireless_examples &amp;gt; bluetooth &amp;gt; ble_fscibb) application from the KW38 SDK as base. FSCI should support UART, SPI and I2C.&lt;/P&gt;
&lt;P&gt;Although I2C should be supported by FSCI, it may not be implemented for usage with Serial Manager (FSCI module uses the Serial Manager on top of a serial interface for communication), and you may need to develop your own implementation of I2C.&lt;/P&gt;
&lt;P&gt;For more information on FSCI, you can refer to the following documentation (inside KW38 SDK docs folder &amp;gt; docs &amp;gt; wireless &amp;gt; Bluetooth):&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;BLE Host Stack FSCI Reference Manual; this reference manual provides a detailed description of the BLE Host Stack serial commands, communication packet structure, and usage of the Framework Serial Communication Interface (FSCI).&lt;/LI&gt;
&lt;LI&gt;BLE Host Stack FSCI Application Programming; this document provides a description for the Kinetis Wireless Host API implementing the FSCI on a peripheral port such as UART, USB and SPI.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;KW38 SDK documentation can be downloaded from the &lt;A href="https://mcuxpresso.nxp.com/en/select" target="_blank"&gt;MCUXpresso SDK Builder&lt;/A&gt;, after building the SDK and when download dialog is shown:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EduardoZamora_0-1692308870254.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236951i2B03519A98873DE1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EduardoZamora_0-1692308870254.png" alt="EduardoZamora_0-1692308870254.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;EduardoZamora_0-1692308870254.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Thu, 17 Aug 2023 21:48:42 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2023-08-17T21:48:42Z</dc:date>
    <item>
      <title>FRDM-KW38 FSCI using I2C</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW38-FSCI-using-I2C/m-p/1706636#M15477</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;My requirement is make BLE pairing using FSCI I2C serial protocol.&lt;BR /&gt;Kindly Some one help me or suggest me any example.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;AjayK&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 12:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW38-FSCI-using-I2C/m-p/1706636#M15477</guid>
      <dc:creator>Ajay1202</dc:creator>
      <dc:date>2023-08-17T12:16:14Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-KW38 FSCI using I2C</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW38-FSCI-using-I2C/m-p/1707053#M15483</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/219236"&gt;@Ajay1202&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;You can use the ble_fsci_black_box (inside wireless_examples &amp;gt; bluetooth &amp;gt; ble_fscibb) application from the KW38 SDK as base. FSCI should support UART, SPI and I2C.&lt;/P&gt;
&lt;P&gt;Although I2C should be supported by FSCI, it may not be implemented for usage with Serial Manager (FSCI module uses the Serial Manager on top of a serial interface for communication), and you may need to develop your own implementation of I2C.&lt;/P&gt;
&lt;P&gt;For more information on FSCI, you can refer to the following documentation (inside KW38 SDK docs folder &amp;gt; docs &amp;gt; wireless &amp;gt; Bluetooth):&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;BLE Host Stack FSCI Reference Manual; this reference manual provides a detailed description of the BLE Host Stack serial commands, communication packet structure, and usage of the Framework Serial Communication Interface (FSCI).&lt;/LI&gt;
&lt;LI&gt;BLE Host Stack FSCI Application Programming; this document provides a description for the Kinetis Wireless Host API implementing the FSCI on a peripheral port such as UART, USB and SPI.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;KW38 SDK documentation can be downloaded from the &lt;A href="https://mcuxpresso.nxp.com/en/select" target="_blank"&gt;MCUXpresso SDK Builder&lt;/A&gt;, after building the SDK and when download dialog is shown:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EduardoZamora_0-1692308870254.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/236951i2B03519A98873DE1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EduardoZamora_0-1692308870254.png" alt="EduardoZamora_0-1692308870254.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;EduardoZamora_0-1692308870254.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Thu, 17 Aug 2023 21:48:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/FRDM-KW38-FSCI-using-I2C/m-p/1707053#M15483</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2023-08-17T21:48:42Z</dc:date>
    </item>
  </channel>
</rss>