<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 ISO14443 device level compatibility with MIFARE</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/ISO14443-device-level-compatibility-with-MIFARE/m-p/1672223#M15180</link>
    <description>&lt;P&gt;I'm aware that there's a standard called ISO 14443 and an associated testing standard that is at a component level (ie PN7462 module).&lt;/P&gt;&lt;P&gt;My question is: if I'm designing a custom version of an existing evaluatoin board (ie PNEV7462C), do I need to test to the ISO standard mentioned for my new antenna size?&lt;/P&gt;&lt;P&gt;Is there a chance we won't successfully communicate with something like an Infineon tag or a MIFARE or something?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;MArko&lt;/P&gt;</description>
    <pubDate>Mon, 19 Jun 2023 23:32:11 GMT</pubDate>
    <dc:creator>meekeech</dc:creator>
    <dc:date>2023-06-19T23:32:11Z</dc:date>
    <item>
      <title>ISO14443 device level compatibility with MIFARE</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/ISO14443-device-level-compatibility-with-MIFARE/m-p/1672223#M15180</link>
      <description>&lt;P&gt;I'm aware that there's a standard called ISO 14443 and an associated testing standard that is at a component level (ie PN7462 module).&lt;/P&gt;&lt;P&gt;My question is: if I'm designing a custom version of an existing evaluatoin board (ie PNEV7462C), do I need to test to the ISO standard mentioned for my new antenna size?&lt;/P&gt;&lt;P&gt;Is there a chance we won't successfully communicate with something like an Infineon tag or a MIFARE or something?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;MArko&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jun 2023 23:32:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/ISO14443-device-level-compatibility-with-MIFARE/m-p/1672223#M15180</guid>
      <dc:creator>meekeech</dc:creator>
      <dc:date>2023-06-19T23:32:11Z</dc:date>
    </item>
    <item>
      <title>Re: ISO14443 device level compatibility with MIFARE</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/ISO14443-device-level-compatibility-with-MIFARE/m-p/1673053#M15186</link>
      <description>&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="es-MX"&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;Thank you for your interest in our products.&lt;/FONT&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="es-MX"&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;ISO14443 is a standard for a type of RFID tag, It isn't required to work with it but, most of the tags that are sold work under it.&lt;/FONT&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="es-MX"&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;This will depend entirely on the tag you will communicate to.&lt;/FONT&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="es-MX"&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;In order to design an antenna please take a look at our Antenna Design Guide.&lt;/FONT&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="es-MX"&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN11706.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN11706.pdf&lt;/A&gt;&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 22:41:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/ISO14443-device-level-compatibility-with-MIFARE/m-p/1673053#M15186</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2023-06-20T22:41:14Z</dc:date>
    </item>
  </channel>
</rss>