<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic QN9090-DK006 example code &amp;amp; UUID in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-DK006-example-code-amp-UUID/m-p/1664654#M15080</link>
    <description>&lt;P&gt;I'm trying to send and receive data over Bluetooth using QN9090-DK006.&lt;BR /&gt;Create numbers with QN9090-DK006 and check the data on the PC side via Bluetooth.&lt;BR /&gt;The sdk I am currently referring to is qn9090dk6_hid_device_bm.&lt;BR /&gt;This is automatically recognized as Mouse on the PC.&lt;BR /&gt;I want it to be recognized as Device instead of Mouse.&lt;BR /&gt;I want to change the UUID setting, but I don't know where it is described.&lt;/P&gt;&lt;P&gt;Is it okay to use the sdk qn9090dk6_hid_device_bm as a reference for the function I want to achieve?&lt;BR /&gt;Please let me know if there is a better sdk sample.&lt;BR /&gt;I would like to know the file and value set for UUID in sdk.&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jun 2023 00:25:48 GMT</pubDate>
    <dc:creator>TM33</dc:creator>
    <dc:date>2023-06-07T00:25:48Z</dc:date>
    <item>
      <title>QN9090-DK006 example code &amp; UUID</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-DK006-example-code-amp-UUID/m-p/1664654#M15080</link>
      <description>&lt;P&gt;I'm trying to send and receive data over Bluetooth using QN9090-DK006.&lt;BR /&gt;Create numbers with QN9090-DK006 and check the data on the PC side via Bluetooth.&lt;BR /&gt;The sdk I am currently referring to is qn9090dk6_hid_device_bm.&lt;BR /&gt;This is automatically recognized as Mouse on the PC.&lt;BR /&gt;I want it to be recognized as Device instead of Mouse.&lt;BR /&gt;I want to change the UUID setting, but I don't know where it is described.&lt;/P&gt;&lt;P&gt;Is it okay to use the sdk qn9090dk6_hid_device_bm as a reference for the function I want to achieve?&lt;BR /&gt;Please let me know if there is a better sdk sample.&lt;BR /&gt;I would like to know the file and value set for UUID in sdk.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 00:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9090-DK006-example-code-amp-UUID/m-p/1664654#M15080</guid>
      <dc:creator>TM33</dc:creator>
      <dc:date>2023-06-07T00:25:48Z</dc:date>
    </item>
    <item>
      <title>回复： QN9090-DK006 example code &amp; UUID</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-DK006-example-code-amp-UUID/m-p/1664938#M15086</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/216387"&gt;@TM33&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for contacting NXP support.&lt;/P&gt;
&lt;P&gt;NXP provides a rich set of sample projects to help with BLE development. If you want to&amp;nbsp;&lt;SPAN&gt;send and receive data over Bluetooth using QN9090-DK006, we believe that Wireless UART is a better DEMO for your requirements.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The application is built to work with another supported platform running the same example or with the Wireless UART from the IoT Toolbox application.&amp;nbsp;With this sample project, you can try to implement data transfer between two QN9090 boards or one board and mobile app.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;For more detailed implementation and usage instructions, as well as for other examples in the SDK, please refer to this document:&amp;nbsp;&lt;U&gt;&lt;EM&gt;Bluetooth Low Energy Demo Applications User's Guide.pdf ,&lt;/EM&gt;&lt;/U&gt;&amp;nbsp; which located at this path:&amp;nbsp;&lt;U&gt;&lt;EM&gt;&lt;STRONG&gt;SDK_Root_Path\docs\wireless\Bluetooth\Bluetooth Low Energy Demo Applications User's Guide.pdf&lt;/STRONG&gt;&lt;/EM&gt;&lt;/U&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;U&gt;&lt;/U&gt;Hope you are doing well!&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Gavin&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 07:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9090-DK006-example-code-amp-UUID/m-p/1664938#M15086</guid>
      <dc:creator>Gavin_Jia</dc:creator>
      <dc:date>2023-06-07T07:28:40Z</dc:date>
    </item>
  </channel>
</rss>