<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Building project on JN5168</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Building-project-on-JN5168/m-p/582664#M1502</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some project, based on 1190-JenNet-IP-Application-Template, and use JN5168.&lt;/P&gt;&lt;P&gt;Now project includes one coordinator and three routers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I change the code for my coordinator, I build the binary file and program coordinator.&lt;/P&gt;&lt;P&gt;But routers refuse to connect to new network and I have to build new binary file for router and reprogram all routers.&lt;/P&gt;&lt;P&gt;Parameters CONFIG_NETWORK_ID, CONFIG_PAN_ID and CONFIG_SCAN_CHANNELS have constant values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please, give me an advice. Which additional parameters have I to do constant to avoid reprogramming all routers in case, when I build the binary file and program only coordinator?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Aug 2016 07:58:03 GMT</pubDate>
    <dc:creator>gibish</dc:creator>
    <dc:date>2016-08-09T07:58:03Z</dc:date>
    <item>
      <title>Building project on JN5168</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Building-project-on-JN5168/m-p/582664#M1502</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some project, based on 1190-JenNet-IP-Application-Template, and use JN5168.&lt;/P&gt;&lt;P&gt;Now project includes one coordinator and three routers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I change the code for my coordinator, I build the binary file and program coordinator.&lt;/P&gt;&lt;P&gt;But routers refuse to connect to new network and I have to build new binary file for router and reprogram all routers.&lt;/P&gt;&lt;P&gt;Parameters CONFIG_NETWORK_ID, CONFIG_PAN_ID and CONFIG_SCAN_CHANNELS have constant values.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please, give me an advice. Which additional parameters have I to do constant to avoid reprogramming all routers in case, when I build the binary file and program only coordinator?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 07:58:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Building-project-on-JN5168/m-p/582664#M1502</guid>
      <dc:creator>gibish</dc:creator>
      <dc:date>2016-08-09T07:58:03Z</dc:date>
    </item>
    <item>
      <title>Re: Building project on JN5168</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Building-project-on-JN5168/m-p/582665#M1503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When you load the program into coordinator device, you have to preserv EEPROM in the setup of programmer. if you don't, you will delete the info about the network, hence the coordinator will not remember its children. Good luck&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Aug 2016 16:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Building-project-on-JN5168/m-p/582665#M1503</guid>
      <dc:creator>janibal</dc:creator>
      <dc:date>2016-08-09T16:11:01Z</dc:date>
    </item>
  </channel>
</rss>