<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 NTAG 5 switch does not work with android app</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/NTAG-5-switch-does-not-work-with-android-app/m-p/1658343#M15014</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have bought an NTAG 5&amp;nbsp; switch a few weeks ago. After I have built the circuit I installed the android app source code (SW5870 from NXP Homepage) with Android Studio on my smartphone (Version 1.1). Unfortunately the button "ALM USE CASE" not exists. That not a problem for me, because I do not need this function. So I wanted to use the button "GPIO USE CASE". I can read my NTAG 5 switch, but I can not write him. The app shows that the switch is described, but in reality it is not, because when I go out of the app and close it and back in, I read out the NTAG again and then the last configured value is not there. It is still the old value there. I also tried to press the Button "SET GPIO/PWM Mode" after writing. There comes then a message that the configuration was successfully taken over and I should restart the NTAG.&lt;BR /&gt;After a power reset unfortunately nothing has changed in the configuration.&lt;/P&gt;&lt;P&gt;Also I tried different smartphones with Android 7, 8 and 12. But&amp;nbsp;all had the same problem.&lt;/P&gt;&lt;P&gt;Can someone please help me and tell me what I am doing wrong?&lt;/P&gt;&lt;P&gt;Many thanks in advance.&lt;/P&gt;&lt;P&gt;Best Regards Niklas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 26 May 2023 10:38:52 GMT</pubDate>
    <dc:creator>Niklas1</dc:creator>
    <dc:date>2023-05-26T10:38:52Z</dc:date>
    <item>
      <title>NTAG 5 switch does not work with android app</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NTAG-5-switch-does-not-work-with-android-app/m-p/1658343#M15014</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have bought an NTAG 5&amp;nbsp; switch a few weeks ago. After I have built the circuit I installed the android app source code (SW5870 from NXP Homepage) with Android Studio on my smartphone (Version 1.1). Unfortunately the button "ALM USE CASE" not exists. That not a problem for me, because I do not need this function. So I wanted to use the button "GPIO USE CASE". I can read my NTAG 5 switch, but I can not write him. The app shows that the switch is described, but in reality it is not, because when I go out of the app and close it and back in, I read out the NTAG again and then the last configured value is not there. It is still the old value there. I also tried to press the Button "SET GPIO/PWM Mode" after writing. There comes then a message that the configuration was successfully taken over and I should restart the NTAG.&lt;BR /&gt;After a power reset unfortunately nothing has changed in the configuration.&lt;/P&gt;&lt;P&gt;Also I tried different smartphones with Android 7, 8 and 12. But&amp;nbsp;all had the same problem.&lt;/P&gt;&lt;P&gt;Can someone please help me and tell me what I am doing wrong?&lt;/P&gt;&lt;P&gt;Many thanks in advance.&lt;/P&gt;&lt;P&gt;Best Regards Niklas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 10:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NTAG-5-switch-does-not-work-with-android-app/m-p/1658343#M15014</guid>
      <dc:creator>Niklas1</dc:creator>
      <dc:date>2023-05-26T10:38:52Z</dc:date>
    </item>
  </channel>
</rss>