<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: QN9090 Post Build Binary Size Error</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1653414#M14982</link>
    <description>&lt;P&gt;Hi Eduardo, thanks for the quick reply.&lt;/P&gt;&lt;P&gt;My project is based off of the wireless_uart_bm project in the QN9090DK6 SDK version 2.6.5. MCUXpresso v11.4.1_6260. I have not modified the python script.&lt;/P&gt;&lt;P&gt;I have added my own modifications to the project and had that working well for several days, then I added an additional source folder to add SEGGER System View support to the project, and that is when the post build script started throwing this error. I have not yet used any functions from the System View source folder I added and there are no build errors. However, when I exclude the System View source folder from my build, the binary size appears to be less than the "stated_size" threshold and there is no error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the stated size?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Gabriel&lt;/P&gt;</description>
    <pubDate>Fri, 19 May 2023 00:26:00 GMT</pubDate>
    <dc:creator>gllake</dc:creator>
    <dc:date>2023-05-19T00:26:00Z</dc:date>
    <item>
      <title>QN9090 Post Build Binary Size Error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1653323#M14979</link>
      <description>&lt;P&gt; &lt;/P&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;My project is running into an error generated by the post-build script dk6_image_tool.py. The error occurs after adding an additional source folder to my project, increasing the flash utilization from 43.20% to 45.08%. I am not sure why increasing the compiled binary size is causing this error, as there is plenty of free space in flash? I can ignore the error, but my board does not work at all after flashing it with the resulting binary--although the source is functionally unchanged. Please see attached for relevant content.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="qn9090-build-console-with-sysview.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/223847iC36D10CC63535621/image-size/medium?v=v2&amp;amp;px=400" role="button" title="qn9090-build-console-with-sysview.PNG" alt="qn9090-build-console-with-sysview.PNG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;qn9090-build-console-with-sysview.PNG&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;/P&gt;&lt;P&gt;Gabriel&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 18 May 2023 20:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1653323#M14979</guid>
      <dc:creator>gllake</dc:creator>
      <dc:date>2023-05-18T20:44:49Z</dc:date>
    </item>
    <item>
      <title>Re: QN9090 Post Build Binary Size Error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1653412#M14981</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/207804"&gt;@gllake&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please provide more details about your project? Are you using any of the example projects from the &lt;A href="https://mcuxpresso.nxp.com/en/select" target="_blank"&gt;QN9090 SDK&lt;/A&gt; as base for your application? How are you modifying the project?&lt;/P&gt;
&lt;P&gt;Which SDK version are you using? What is the version of MCUXpresso you are using?&lt;/P&gt;
&lt;P&gt;By any chance, did you modify the dk6_image_tool.py script?&lt;/P&gt;
&lt;P&gt;Any additional information that could help me to try to reproduce this issue on my side is appreciated.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Fri, 19 May 2023 00:14:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1653412#M14981</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2023-05-19T00:14:06Z</dc:date>
    </item>
    <item>
      <title>Re: QN9090 Post Build Binary Size Error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1653414#M14982</link>
      <description>&lt;P&gt;Hi Eduardo, thanks for the quick reply.&lt;/P&gt;&lt;P&gt;My project is based off of the wireless_uart_bm project in the QN9090DK6 SDK version 2.6.5. MCUXpresso v11.4.1_6260. I have not modified the python script.&lt;/P&gt;&lt;P&gt;I have added my own modifications to the project and had that working well for several days, then I added an additional source folder to add SEGGER System View support to the project, and that is when the post build script started throwing this error. I have not yet used any functions from the System View source folder I added and there are no build errors. However, when I exclude the System View source folder from my build, the binary size appears to be less than the "stated_size" threshold and there is no error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What is the stated size?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Gabriel&lt;/P&gt;</description>
      <pubDate>Fri, 19 May 2023 00:26:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1653414#M14982</guid>
      <dc:creator>gllake</dc:creator>
      <dc:date>2023-05-19T00:26:00Z</dc:date>
    </item>
    <item>
      <title>Re: QN9090 Post Build Binary Size Error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1655029#M14987</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Could you please try increasing the __app_stated_size__? This symbol should be found in project properties &amp;gt; C/C++ Build &amp;gt; Settings &amp;gt; MCU Linker &amp;gt; Miscellaneous.&lt;BR /&gt;&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EduardoZamora_0-1684780748486.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/224287i9FA6BC7294783C9F/image-size/large?v=v2&amp;amp;px=999" role="button" title="EduardoZamora_0-1684780748486.png" alt="EduardoZamora_0-1684780748486.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;EduardoZamora_0-1684780748486.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please consider that stated size must be a multiple of 8k (i.e., 303104).&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 22 May 2023 18:41:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1655029#M14987</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2023-05-22T18:41:25Z</dc:date>
    </item>
    <item>
      <title>Re: QN9090 Post Build Binary Size Error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1655093#M14988</link>
      <description>&lt;P&gt;I changed it to 311296 and the error is gone!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;Gabriel&lt;/P&gt;</description>
      <pubDate>Tue, 23 May 2023 00:16:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9090-Post-Build-Binary-Size-Error/m-p/1655093#M14988</guid>
      <dc:creator>gllake</dc:creator>
      <dc:date>2023-05-23T00:16:54Z</dc:date>
    </item>
  </channel>
</rss>