<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Please give me some opinions or doc about testing UWB AOA in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Please-give-me-some-opinions-or-doc-about-testing-UWB-AOA/m-p/1632936#M14862</link>
    <description>&lt;P&gt;Hi community:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am verifying the AOA function of device which has equiped uwb IC SR100T. i used nxp_uwb_test.apk to test aoa function, and the test steps as follow:&lt;/P&gt;&lt;P&gt;1. Used two devices, adopt way of one to one wireless communication, both of them install&amp;nbsp;nxp_uwb_test.apk to test and config previous condition of uwb AOA&lt;/P&gt;&lt;P&gt;2. One was set intititor and other was set responder&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;Run the inititor ranging callback and then run the responder side to respond to the inititor side&lt;/P&gt;&lt;P&gt;4. The responder device circles the inititor device around the center of the sphere，and i will observe changes of AOA from the apk UI&lt;/P&gt;&lt;P&gt;As a result, i didn't found some changes of aoa from UI. due to lacking of some opinions or doc, i can't locate reason why angle of arrivel no change with responder moving, so i hopefully want to get some advice from forums to fix this issue.thanks everybody!&lt;/P&gt;&lt;P&gt;PS:The software package used is called&amp;nbsp;UWB01_SW_Android_S_SW_D31.zip&lt;/P&gt;</description>
    <pubDate>Thu, 13 Apr 2023 07:56:33 GMT</pubDate>
    <dc:creator>bluebank</dc:creator>
    <dc:date>2023-04-13T07:56:33Z</dc:date>
    <item>
      <title>Please give me some opinions or doc about testing UWB AOA</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Please-give-me-some-opinions-or-doc-about-testing-UWB-AOA/m-p/1632936#M14862</link>
      <description>&lt;P&gt;Hi community:&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am verifying the AOA function of device which has equiped uwb IC SR100T. i used nxp_uwb_test.apk to test aoa function, and the test steps as follow:&lt;/P&gt;&lt;P&gt;1. Used two devices, adopt way of one to one wireless communication, both of them install&amp;nbsp;nxp_uwb_test.apk to test and config previous condition of uwb AOA&lt;/P&gt;&lt;P&gt;2. One was set intititor and other was set responder&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;Run the inititor ranging callback and then run the responder side to respond to the inititor side&lt;/P&gt;&lt;P&gt;4. The responder device circles the inititor device around the center of the sphere，and i will observe changes of AOA from the apk UI&lt;/P&gt;&lt;P&gt;As a result, i didn't found some changes of aoa from UI. due to lacking of some opinions or doc, i can't locate reason why angle of arrivel no change with responder moving, so i hopefully want to get some advice from forums to fix this issue.thanks everybody!&lt;/P&gt;&lt;P&gt;PS:The software package used is called&amp;nbsp;UWB01_SW_Android_S_SW_D31.zip&lt;/P&gt;</description>
      <pubDate>Thu, 13 Apr 2023 07:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Please-give-me-some-opinions-or-doc-about-testing-UWB-AOA/m-p/1632936#M14862</guid>
      <dc:creator>bluebank</dc:creator>
      <dc:date>2023-04-13T07:56:33Z</dc:date>
    </item>
  </channel>
</rss>