<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: Using UART0 as Wakeup Source JN5189</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Using-UART0-as-Wakeup-Source-JN5189/m-p/1631491#M14834</link>
    <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you just want to wake up on any signal on the RX port, you can use GPIO interrupts to capture the start bit.&lt;/P&gt;&lt;P&gt;My code uses the GINT interrupt and can treat the change in PIO9 (UART0 RXD) as a wake-up source. Sorry, I cannot provide a simple sample code.&lt;/P&gt;&lt;P&gt;One thing is required before sleep: POWER_WAKEUPSRC_IO bit must be set as the wake-up interrupt source, passing to&amp;nbsp;POWER_EnterPowerMode().&lt;/P&gt;</description>
    <pubDate>Tue, 11 Apr 2023 17:43:35 GMT</pubDate>
    <dc:creator>usaygo</dc:creator>
    <dc:date>2023-04-11T17:43:35Z</dc:date>
    <item>
      <title>Using UART0 as Wakeup Source JN5189</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Using-UART0-as-Wakeup-Source-JN5189/m-p/1630148#M14819</link>
      <description>&lt;P&gt;I'm trying to get a JN5189, configured as a SED, to go into power-down mode and wake up from a UART0 message. Is there any documentation or Application Note which describes how to do this?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 09 Apr 2023 21:46:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Using-UART0-as-Wakeup-Source-JN5189/m-p/1630148#M14819</guid>
      <dc:creator>Lukas10999</dc:creator>
      <dc:date>2023-04-09T21:46:49Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART0 as Wakeup Source JN5189</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Using-UART0-as-Wakeup-Source-JN5189/m-p/1630767#M14824</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/212806"&gt;@Lukas10999&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;Usually, Zigbee SED should use these methods to wake up:&lt;/P&gt;
&lt;UL type="disc"&gt;
&lt;LI&gt;GPIO&lt;/LI&gt;
&lt;LI&gt;Cyclic (Timer)&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;If you need to send data to a SED using UART, I suggest taking advantage of the ON interval of the device. You can use JN-AN-1246 Zigbee 3 Sensors as reference, the Occupancy Sensor can be configured as a sleeping End Device.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Apr 2023 23:18:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Using-UART0-as-Wakeup-Source-JN5189/m-p/1630767#M14824</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2023-04-10T23:18:59Z</dc:date>
    </item>
    <item>
      <title>Re: Using UART0 as Wakeup Source JN5189</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Using-UART0-as-Wakeup-Source-JN5189/m-p/1631491#M14834</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you just want to wake up on any signal on the RX port, you can use GPIO interrupts to capture the start bit.&lt;/P&gt;&lt;P&gt;My code uses the GINT interrupt and can treat the change in PIO9 (UART0 RXD) as a wake-up source. Sorry, I cannot provide a simple sample code.&lt;/P&gt;&lt;P&gt;One thing is required before sleep: POWER_WAKEUPSRC_IO bit must be set as the wake-up interrupt source, passing to&amp;nbsp;POWER_EnterPowerMode().&lt;/P&gt;</description>
      <pubDate>Tue, 11 Apr 2023 17:43:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Using-UART0-as-Wakeup-Source-JN5189/m-p/1631491#M14834</guid>
      <dc:creator>usaygo</dc:creator>
      <dc:date>2023-04-11T17:43:35Z</dc:date>
    </item>
  </channel>
</rss>