<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Fxth 8700 in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Fxth-8700/m-p/356584#M146</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the chip Fxth8700 for a TPMS project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need help to design the matching network for the antenna (433MHz) , because I'm not expert on that field.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1) Why there is L1 between Vdd and the RF pin? Which value should it have?&lt;/P&gt;&lt;P&gt;Q2) Has the RF pin a source impedance of 50 ohms? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Riccardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 07 Feb 2015 16:05:40 GMT</pubDate>
    <dc:creator>riccardocescato</dc:creator>
    <dc:date>2015-02-07T16:05:40Z</dc:date>
    <item>
      <title>Fxth 8700</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Fxth-8700/m-p/356584#M146</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the chip Fxth8700 for a TPMS project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need help to design the matching network for the antenna (433MHz) , because I'm not expert on that field.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Q1) Why there is L1 between Vdd and the RF pin? Which value should it have?&lt;/P&gt;&lt;P&gt;Q2) Has the RF pin a source impedance of 50 ohms? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Riccardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Feb 2015 16:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Fxth-8700/m-p/356584#M146</guid>
      <dc:creator>riccardocescato</dc:creator>
      <dc:date>2015-02-07T16:05:40Z</dc:date>
    </item>
    <item>
      <title>Re: Fxth 8700</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Fxth-8700/m-p/356585#M147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ricardo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to Xtrinsic FXTH87 Family Evaluation Design Reference Manual (&lt;A href="http://cache.freescale.com/files/sensors/doc/ref_manual/FXTH87EDRM.pdf"&gt;http://cache.freescale.com/files/sensors/doc/ref_manual/FXTH87EDRM.pdf&lt;/A&gt; ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In chapter 3.2.2. you will find recommended values of components in matching network.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your question: in simplest words the function of L1 is to "separate" RF from Vdd at working frequency (315 or 432 MHz).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Wlodek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Feb 2015 12:47:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Fxth-8700/m-p/356585#M147</guid>
      <dc:creator>Wlodek_D_</dc:creator>
      <dc:date>2015-02-09T12:47:36Z</dc:date>
    </item>
    <item>
      <title>Re: Fxth 8700</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Fxth-8700/m-p/356586#M148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I design the PCB as the referenc, but the matching is not good....&lt;/P&gt;&lt;P&gt;Set the input power to 0dm,&amp;nbsp;&amp;nbsp; connect it to Spectrum Analyzer by coaxial directly , just -40dBm power is tested.&lt;/P&gt;&lt;P&gt;It sugest the matching is so bad...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to improve?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Mar 2016 14:58:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Fxth-8700/m-p/356586#M148</guid>
      <dc:creator>yapingwang</dc:creator>
      <dc:date>2016-03-10T14:58:04Z</dc:date>
    </item>
  </channel>
</rss>