<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 MFRC522 not switchable to UART</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/MFRC522-not-switchable-to-UART/m-p/1586305#M14410</link>
    <description>&lt;P&gt;I am trying to use the UART interface instead of the SPI with MFRC522.&lt;/P&gt;&lt;P&gt;I set the EA pin and i2c to GND, but the communication is still working in SPI, I am not able to use UART.&lt;/P&gt;&lt;P&gt;Pin are measured with multimeter and value are ok.&lt;/P&gt;&lt;P&gt;Tried a reset with dedicated pin but still working is SPI&amp;nbsp; and not UART.&lt;/P&gt;&lt;P&gt;Is there any suggestion?&lt;/P&gt;&lt;P&gt;Thank you for support&lt;/P&gt;</description>
    <pubDate>Fri, 20 Jan 2023 22:55:00 GMT</pubDate>
    <dc:creator>PaoloArtuso</dc:creator>
    <dc:date>2023-01-20T22:55:00Z</dc:date>
    <item>
      <title>MFRC522 not switchable to UART</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MFRC522-not-switchable-to-UART/m-p/1586305#M14410</link>
      <description>&lt;P&gt;I am trying to use the UART interface instead of the SPI with MFRC522.&lt;/P&gt;&lt;P&gt;I set the EA pin and i2c to GND, but the communication is still working in SPI, I am not able to use UART.&lt;/P&gt;&lt;P&gt;Pin are measured with multimeter and value are ok.&lt;/P&gt;&lt;P&gt;Tried a reset with dedicated pin but still working is SPI&amp;nbsp; and not UART.&lt;/P&gt;&lt;P&gt;Is there any suggestion?&lt;/P&gt;&lt;P&gt;Thank you for support&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 22:55:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MFRC522-not-switchable-to-UART/m-p/1586305#M14410</guid>
      <dc:creator>PaoloArtuso</dc:creator>
      <dc:date>2023-01-20T22:55:00Z</dc:date>
    </item>
  </channel>
</rss>