<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Timer management in a BLE connection in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Timer-management-in-a-BLE-connection/m-p/1572699#M14197</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;According to the Connectivity Framework Reference Manual (inside KW38 docs folder &amp;gt; docs &amp;gt; wireless &amp;gt; common), &lt;SPAN&gt;TMR_StartLowPowerTimer&lt;/SPAN&gt; starts a low-power timer which can operate across all power modes, including low-leakage modes. This timer is necessary because MCU can enter low-power mode if there are only active low-power timers.&lt;/P&gt;
&lt;P&gt;Taking a look at TimersManager.h, valid range for &lt;SPAN&gt;gTmrApplicationTimers_c&amp;nbsp;&lt;/SPAN&gt;macro should be user defined depending on the timers needed by the application.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Tue, 20 Dec 2022 19:53:24 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2022-12-20T19:53:24Z</dc:date>
    <item>
      <title>Timer management in a BLE connection</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Timer-management-in-a-BLE-connection/m-p/1572522#M14195</link>
      <description>&lt;P&gt;I have 2 questions related to TimerManager in kw38 ble sample app 'frdmkw38_adv_ext_peripheral_bm'.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1.&lt;/STRONG&gt; Sample example uses 'TMR_StartLowPowerTimer' API. What is the context of LowPower in this API name?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2.&lt;/STRONG&gt; gTmrApplicationTimers_c flag is defined and set its value to 4 in app_preinclude.h file. Can i change value of this flag? If yes, what is the maximum limit?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Nidhin&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 12:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Timer-management-in-a-BLE-connection/m-p/1572522#M14195</guid>
      <dc:creator>nidhintomy</dc:creator>
      <dc:date>2022-12-20T12:06:35Z</dc:date>
    </item>
    <item>
      <title>Re: Timer management in a BLE connection</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Timer-management-in-a-BLE-connection/m-p/1572699#M14197</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;According to the Connectivity Framework Reference Manual (inside KW38 docs folder &amp;gt; docs &amp;gt; wireless &amp;gt; common), &lt;SPAN&gt;TMR_StartLowPowerTimer&lt;/SPAN&gt; starts a low-power timer which can operate across all power modes, including low-leakage modes. This timer is necessary because MCU can enter low-power mode if there are only active low-power timers.&lt;/P&gt;
&lt;P&gt;Taking a look at TimersManager.h, valid range for &lt;SPAN&gt;gTmrApplicationTimers_c&amp;nbsp;&lt;/SPAN&gt;macro should be user defined depending on the timers needed by the application.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 20 Dec 2022 19:53:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Timer-management-in-a-BLE-connection/m-p/1572699#M14197</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2022-12-20T19:53:24Z</dc:date>
    </item>
  </channel>
</rss>