<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: JN5169 programming error</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567374#M1406</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David, how do I select tje jn5168? in the JN-AN-1218 there are only jn5169 .bin files&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 Mar 2019 09:45:22 GMT</pubDate>
    <dc:creator>dirk_van_grunsv</dc:creator>
    <dc:date>2019-03-04T09:45:22Z</dc:date>
    <item>
      <title>JN5169 programming error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567368#M1400</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recently received my JN516x-EK004 eval kit.&amp;nbsp; I have installed the BeyondStudio environment and was able to successfully read the two DR1178 devices that came with the kit.&amp;nbsp; I pulled the JN-AN-1223 application note zip from the website and so I could take a look at the Zigbee Gateway User Interface project.&amp;nbsp; I then decided to load the DimmableLight_JN5169_DR1175_LED_EXP_MONO.bin file onto my devices.&amp;nbsp; I did this on the first one with the EEPROM set to Erase PDM.&amp;nbsp; It seems to have successfully programmed but I can no longer read that device.&amp;nbsp; I did the second one but set the EEPROM to Preserve EEPROM and that one seems to be fine.&amp;nbsp; I can connect to it with the previously mentioned Zigbee Gateway User Interface and I can still read the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find a way to recover my first device.&amp;nbsp; I have already spent hours digging through documentation trying to figure it out.&amp;nbsp; When I use the JN51xx Production Flash Programmer it comes back with error: reading chip ID - check cabling and power.&amp;nbsp; I'm hoping someone can explain what I've done and how I can recover the chip.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Aug 2016 00:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567368#M1400</guid>
      <dc:creator>rkoontz</dc:creator>
      <dc:date>2016-08-04T00:50:51Z</dc:date>
    </item>
    <item>
      <title>Re: JN5169 programming error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567369#M1401</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;me too. Who can help we recover the chip? &amp;nbsp;tks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 May 2017 07:41:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567369#M1401</guid>
      <dc:creator>hoangvucuong</dc:creator>
      <dc:date>2017-05-30T07:41:31Z</dc:date>
    </item>
    <item>
      <title>Re: JN5169 programming error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567370#M1402</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just started experimenting with JN5168-001-M00 Modules for my master thesis and now I have just the same problem. At first I can read the Device Info like shown and everything is fine&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Info.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21282i908CE3FBEF62CDCB/image-size/large?v=v2&amp;amp;px=999" role="button" title="Info.JPG" alt="Info.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But when I want to program I get the warning "The loaded image does not appear to be compatible with the connected device. Continue?"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Incompatible.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21328i2F81D518B77D854A/image-size/large?v=v2&amp;amp;px=999" role="button" title="Incompatible.JPG" alt="Incompatible.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;If I program anyway the Device Info can't be read out anymore.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please... I need some help and can't get any further. I would be so happy If I could get some answers from you :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2017 11:20:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567370#M1402</guid>
      <dc:creator>martinpannenbae</dc:creator>
      <dc:date>2017-06-07T11:20:18Z</dc:date>
    </item>
    <item>
      <title>Re: JN5169 programming error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567371#M1403</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Make sure you're flashing it with "jn5168" binary not "jn5169"&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Jul 2017 20:06:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567371#M1403</guid>
      <dc:creator>davidashraf</dc:creator>
      <dc:date>2017-07-10T20:06:17Z</dc:date>
    </item>
    <item>
      <title>Re: JN5169 programming error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567372#M1404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer David. Actually this caused the warning message... Sorry I'm just getting into it :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Furthermore I found out that the re-progamming issue had something to do with a pull-down resistor I used to set the device into programming mode. After connecting SPIMISO directly to GND without the resistor it just works fine. Seems like there is a small current flowing from the pin in programming Mode leading to a voltage drop over the pull-down resistor, high enough to keep the device from getting into programming mode&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 07:39:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567372#M1404</guid>
      <dc:creator>martinpannenbae</dc:creator>
      <dc:date>2017-07-11T07:39:31Z</dc:date>
    </item>
    <item>
      <title>Re: JN5169 programming error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567373#M1405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am glad it worked:)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jul 2017 09:46:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567373#M1405</guid>
      <dc:creator>davidashraf</dc:creator>
      <dc:date>2017-07-11T09:46:09Z</dc:date>
    </item>
    <item>
      <title>Re: JN5169 programming error</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567374#M1406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David, how do I select tje jn5168? in the JN-AN-1218 there are only jn5169 .bin files&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Mar 2019 09:45:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5169-programming-error/m-p/567374#M1406</guid>
      <dc:creator>dirk_van_grunsv</dc:creator>
      <dc:date>2019-03-04T09:45:22Z</dc:date>
    </item>
  </channel>
</rss>