<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックKW38 interrupt handler</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/KW38-interrupt-handler/m-p/1545935#M13895</link>
    <description>&lt;P&gt;Hello to everyone,&lt;/P&gt;&lt;P&gt;I need an help to understand how to use the interrupt in the KW38 device.&lt;/P&gt;&lt;P&gt;starting with the evaluation board FRDM-KW38 and the project frdmkw38_lp_bm (the low power example) I'm trying just to add an interrupt fired from the pin PTA19, on the falling edge, without success.&lt;/P&gt;&lt;P&gt;Could someone please help me?&lt;/P&gt;</description>
    <pubDate>Sun, 30 Oct 2022 23:58:47 GMT</pubDate>
    <dc:creator>IlDaniAndre</dc:creator>
    <dc:date>2022-10-30T23:58:47Z</dc:date>
    <item>
      <title>KW38 interrupt handler</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW38-interrupt-handler/m-p/1545935#M13895</link>
      <description>&lt;P&gt;Hello to everyone,&lt;/P&gt;&lt;P&gt;I need an help to understand how to use the interrupt in the KW38 device.&lt;/P&gt;&lt;P&gt;starting with the evaluation board FRDM-KW38 and the project frdmkw38_lp_bm (the low power example) I'm trying just to add an interrupt fired from the pin PTA19, on the falling edge, without success.&lt;/P&gt;&lt;P&gt;Could someone please help me?&lt;/P&gt;</description>
      <pubDate>Sun, 30 Oct 2022 23:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW38-interrupt-handler/m-p/1545935#M13895</guid>
      <dc:creator>IlDaniAndre</dc:creator>
      <dc:date>2022-10-30T23:58:47Z</dc:date>
    </item>
  </channel>
</rss>