<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: KW36 FLASH MEMORY DEVICE USAGE ?</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1539767#M13839</link>
    <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200888"&gt;@EduardoZamora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I looked on that documents. And i didn't get any clarity. I successfully used NVM to write data. But no idea where it is stored.&lt;/P&gt;&lt;P&gt;Can you please clarify is there any internal NVM is used?&lt;/P&gt;&lt;P&gt;Is there any document related to how many bytes of data can be stored into the internal NVM, if it exists?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Nidhin&lt;/P&gt;</description>
    <pubDate>Wed, 19 Oct 2022 05:27:18 GMT</pubDate>
    <dc:creator>nidhintomy</dc:creator>
    <dc:date>2022-10-19T05:27:18Z</dc:date>
    <item>
      <title>KW36 FLASH MEMORY DEVICE USAGE ?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1538097#M13813</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot (65).jpg" style="width: 757px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/196849i7870E1DEED5EBD01/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot (65).jpg" alt="Screenshot (65).jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In pin_mux.c file of ble projects "BOARD_InitSPI()" is defined.&lt;/P&gt;&lt;P&gt;1. Is this function is used for access to &lt;STRONG&gt;SPI Flash&lt;/STRONG&gt;?&lt;/P&gt;&lt;P&gt;2. When searching reference, the spi function is never getting called in the project(temp_sens). "App_NvmWrite()" is used for writing data into &lt;STRONG&gt;NVM&lt;/STRONG&gt; . Also bond data is stored into &lt;STRONG&gt;NVM&lt;/STRONG&gt; .&lt;/P&gt;&lt;P&gt;If&amp;nbsp;"BOARD_InitSPI()" is not getting invoked, then where is all &lt;STRONG&gt;NVM&lt;/STRONG&gt; data stored?&lt;/P&gt;&lt;P&gt;3. Is BLE Stack using spi flash ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Nidhin&lt;/P&gt;</description>
      <pubDate>Sat, 15 Oct 2022 11:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1538097#M13813</guid>
      <dc:creator>nidhintomy</dc:creator>
      <dc:date>2022-10-15T11:17:14Z</dc:date>
    </item>
    <item>
      <title>Re: KW36 FLASH MEMORY DEVICE USAGE ?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1538795#M13820</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/194348"&gt;@nidhintomy&lt;/a&gt;&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;void BOARD_InitSPI(void) configures pin routing and optionally pin electrical features. SPI flash should be connected to&amp;nbsp; PTC16 (SPI0_SCK), PTC17 (SPI0_SOUT), PTC18 (SPI0_SIN) and PTC19 (SPI0_PCS0); please verify this configuration in your source code. You can find more information about SPI API in MCUXpresso SDK API Reference Manual_MKW36Z4 (inside KW36 SDK documentation folder &amp;gt; docs), Chapter 11: DSPI Serial Peripheral Interface Driver&lt;/P&gt;
&lt;P&gt;SPI flash is intended for Over-the-Air Programming (OTAP) or for storing non-volatile system data, or parameters. When NVM is enabled, it is used as non-volatile storage management by the host stack, and as you mentioned, it could be used to store bonding data. For more information about memory configuration, please consult the &lt;A href="https://www.nxp.com/webapp/Download?colCode=MKW36A512RM" target="_blank" rel="noopener"&gt;MKW36/35/34 Reference Manual&lt;/A&gt;, Chapter 4.6 Memories and memory interfaces; and Bluetooth Low Energy Application Developer Guide, Chapter 2.3 Non-volatile Memory (NVM) access.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Oct 2022 17:08:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1538795#M13820</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2022-10-18T17:08:20Z</dc:date>
    </item>
    <item>
      <title>Re: KW36 FLASH MEMORY DEVICE USAGE ?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1539186#M13826</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200888"&gt;@EduardoZamora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Glad to hear from you. I am fine.&lt;/P&gt;&lt;P&gt;I want some clarification.&lt;/P&gt;&lt;P&gt;1. Is 'frdmkw36_wireless_examples_bluetooth_temp_sens_bm' actually uses SPI flash ? Because the 'BOARD_InitSPI()' function never get invoked.&lt;/P&gt;&lt;P&gt;2. Is KW36 has an internal memory to store bonded data or data stored by 'App_NvmWrite()' ? If yes, is there any document related to that memory ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Nidhin&lt;/P&gt;</description>
      <pubDate>Tue, 18 Oct 2022 10:10:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1539186#M13826</guid>
      <dc:creator>nidhintomy</dc:creator>
      <dc:date>2022-10-18T10:10:03Z</dc:date>
    </item>
    <item>
      <title>Re: KW36 FLASH MEMORY DEVICE USAGE ?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1539526#M13831</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Temperature sensor may not be using SPI flash. You can find some information about FlexNVM in the MKW36/35/34 Reference Manual, Chapter 4.6 Memories and memory interfaces; and in Bluetooth Low Energy Application Developer Guide, Chapter 2.3 Non-volatile Memory (NVM) access.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Tue, 18 Oct 2022 17:09:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1539526#M13831</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2022-10-18T17:09:04Z</dc:date>
    </item>
    <item>
      <title>Re: KW36 FLASH MEMORY DEVICE USAGE ?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1539767#M13839</link>
      <description>&lt;P&gt;HI &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200888"&gt;@EduardoZamora&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I looked on that documents. And i didn't get any clarity. I successfully used NVM to write data. But no idea where it is stored.&lt;/P&gt;&lt;P&gt;Can you please clarify is there any internal NVM is used?&lt;/P&gt;&lt;P&gt;Is there any document related to how many bytes of data can be stored into the internal NVM, if it exists?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Nidhin&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 05:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1539767#M13839</guid>
      <dc:creator>nidhintomy</dc:creator>
      <dc:date>2022-10-19T05:27:18Z</dc:date>
    </item>
    <item>
      <title>Re: KW36 FLASH MEMORY DEVICE USAGE ?</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1540176#M13843</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Could you please confirm if information shown in section 4.6.1.1 Flash Memory Sizes is helpful for you? Figures 4-22, 4-23 and 4-24 describe the memory distribution, sizes and addresses for different memory configurations, including FlexNVM partitions.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Oct 2022 15:20:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/KW36-FLASH-MEMORY-DEVICE-USAGE/m-p/1540176#M13843</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2022-10-19T15:20:31Z</dc:date>
    </item>
  </channel>
</rss>