<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Soft reset delay at FXTH8715 in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Soft-reset-delay-at-FXTH8715/m-p/1528445#M13744</link>
    <description>&lt;P&gt;Hi friend,&lt;/P&gt;&lt;P&gt;I used the FXTH8715 and periodically reset the LF module with a soft reset (with LFCTL1_SRES = SET).&lt;BR /&gt;Do I need to delay after LFCTL1_SRES = SET? If yes, how much delay might it be? I set all LF registers after soft reset. Then enter STOP1 mode. (vfnSetSTOPMode(STOP1))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best wishes&lt;/P&gt;&lt;P&gt;Ted Wu&lt;/P&gt;</description>
    <pubDate>Tue, 27 Sep 2022 02:11:45 GMT</pubDate>
    <dc:creator>tedwu1</dc:creator>
    <dc:date>2022-09-27T02:11:45Z</dc:date>
    <item>
      <title>Soft reset delay at FXTH8715</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Soft-reset-delay-at-FXTH8715/m-p/1528445#M13744</link>
      <description>&lt;P&gt;Hi friend,&lt;/P&gt;&lt;P&gt;I used the FXTH8715 and periodically reset the LF module with a soft reset (with LFCTL1_SRES = SET).&lt;BR /&gt;Do I need to delay after LFCTL1_SRES = SET? If yes, how much delay might it be? I set all LF registers after soft reset. Then enter STOP1 mode. (vfnSetSTOPMode(STOP1))&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best wishes&lt;/P&gt;&lt;P&gt;Ted Wu&lt;/P&gt;</description>
      <pubDate>Tue, 27 Sep 2022 02:11:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Soft-reset-delay-at-FXTH8715/m-p/1528445#M13744</guid>
      <dc:creator>tedwu1</dc:creator>
      <dc:date>2022-09-27T02:11:45Z</dc:date>
    </item>
    <item>
      <title>Re: Soft reset delay at FXTH8715</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Soft-reset-delay-at-FXTH8715/m-p/1531576#M13766</link>
      <description>&lt;P&gt;Hi Ted,&lt;/P&gt;
&lt;P&gt;I have been informed that my colleague Camille already answered this question.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For reference, the answer is yes, a delay is necessary. More information can be found in section 5.3 of AN4391:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN4391" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=AN4391&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Tomas&lt;/P&gt;</description>
      <pubDate>Mon, 03 Oct 2022 10:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Soft-reset-delay-at-FXTH8715/m-p/1531576#M13766</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2022-10-03T10:46:30Z</dc:date>
    </item>
  </channel>
</rss>