<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: pn5180 documentation</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/pn5180-documentation/m-p/1521609#M13690</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206177"&gt;@Splatspeed&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you don't want to use NXP library to develop, then two suggestions for reference:&lt;/P&gt;
&lt;P&gt;1. Between Master and PN518 is the SPI interface, there is a standard SPI communication protocol, no special application description here. PN5180 datasheet is open source. For PN5180 Antenna design, you can refer AN11740.&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp;Between PN518 and Tag, this application varies according to the tag.&amp;nbsp;If it is NXP's tag, you can download the relevant development documents from the official website.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;kelly&lt;/P&gt;</description>
    <pubDate>Wed, 14 Sep 2022 03:51:59 GMT</pubDate>
    <dc:creator>KaiLi</dc:creator>
    <dc:date>2022-09-14T03:51:59Z</dc:date>
    <item>
      <title>pn5180 documentation</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/pn5180-documentation/m-p/1521114#M13683</link>
      <description>&lt;P&gt;i want to do a uart replacement with 2 of these devices, but i need application notes for doing this without your libraries with 2 powered devices. a flow chart of the messages sent to the NXP chip would be great to do this&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thx in advance Sean&lt;/P&gt;</description>
      <pubDate>Tue, 13 Sep 2022 08:58:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/pn5180-documentation/m-p/1521114#M13683</guid>
      <dc:creator>Splatspeed</dc:creator>
      <dc:date>2022-09-13T08:58:39Z</dc:date>
    </item>
    <item>
      <title>Re: pn5180 documentation</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/pn5180-documentation/m-p/1521609#M13690</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206177"&gt;@Splatspeed&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you don't want to use NXP library to develop, then two suggestions for reference:&lt;/P&gt;
&lt;P&gt;1. Between Master and PN518 is the SPI interface, there is a standard SPI communication protocol, no special application description here. PN5180 datasheet is open source. For PN5180 Antenna design, you can refer AN11740.&lt;/P&gt;
&lt;P&gt;2.&amp;nbsp;Between PN518 and Tag, this application varies according to the tag.&amp;nbsp;If it is NXP's tag, you can download the relevant development documents from the official website.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;kelly&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 03:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/pn5180-documentation/m-p/1521609#M13690</guid>
      <dc:creator>KaiLi</dc:creator>
      <dc:date>2022-09-14T03:51:59Z</dc:date>
    </item>
  </channel>
</rss>