<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Zigbee network without NFC in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/Zigbee-network-without-NFC/m-p/559367#M1365</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using JN516x-EK004 Evaluation Kit with JN5169 modules. I am trying to make a prototype with ZigBee network using the elements from the kit, but without NFC commissioning.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any demo or example code that could be appropriate as a starting point? So far I failed to find one, or to modify the default supplied demo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;Aleks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Aug 2016 21:03:06 GMT</pubDate>
    <dc:creator>salewtg</dc:creator>
    <dc:date>2016-08-02T21:03:06Z</dc:date>
    <item>
      <title>Zigbee network without NFC</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Zigbee-network-without-NFC/m-p/559367#M1365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using JN516x-EK004 Evaluation Kit with JN5169 modules. I am trying to make a prototype with ZigBee network using the elements from the kit, but without NFC commissioning.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any demo or example code that could be appropriate as a starting point? So far I failed to find one, or to modify the default supplied demo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;Aleks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2016 21:03:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Zigbee-network-without-NFC/m-p/559367#M1365</guid>
      <dc:creator>salewtg</dc:creator>
      <dc:date>2016-08-02T21:03:06Z</dc:date>
    </item>
    <item>
      <title>Re: Zigbee network without NFC</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/Zigbee-network-without-NFC/m-p/559368#M1366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;1) Did you try looking into the JN-AN-1189 app note? It is similar to JN-AN-1221, but is meant for JN516x-EK001 kit and does not use NFC commissioning. It uses EZ-mode commissioning.&lt;/P&gt;&lt;P&gt;2) In the JN-AN-1221 &amp;nbsp;doc they do mention that you can do commissioning without using NFC, but I have not gone into it very deeply yet.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 20:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/Zigbee-network-without-NFC/m-p/559368#M1366</guid>
      <dc:creator>navdeepsinghgil</dc:creator>
      <dc:date>2016-10-12T20:32:59Z</dc:date>
    </item>
  </channel>
</rss>