<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 Re: MMZ09332BT1 R1/R2 for 3.3V / 433MHz</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1-R1-R2-for-3-3V-433MHz/m-p/1511043#M13582</link>
    <description>&lt;P&gt;In a post about&amp;nbsp;&lt;SPAN class=""&gt;MMZ25332B you mentioned that you have a&amp;nbsp;&lt;SPAN&gt;guide for adjusting bias resistors with Vdd=5.0V.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Do you have such a guide also for the&amp;nbsp;MMZ09332BT1 for 5V or better in my case 3.3V?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;If so, is it possible to get it?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Thank you in advance&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Thomas&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 24 Aug 2022 15:23:09 GMT</pubDate>
    <dc:creator>Thomas_</dc:creator>
    <dc:date>2022-08-24T15:23:09Z</dc:date>
    <item>
      <title>MMZ09332BT1 R1/R2 for 3.3V / 433MHz</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1-R1-R2-for-3-3V-433MHz/m-p/766659#M4647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How are R1/R2 calculated?&lt;/P&gt;&lt;P&gt;Does gain depends on them?&lt;/P&gt;&lt;P&gt;Suggested values for 3.3V operation in order to get max power output?&lt;/P&gt;&lt;P&gt;Schematic is:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17902iC1DBEC63B9678463/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Apr 2018 00:48:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1-R1-R2-for-3-3V-433MHz/m-p/766659#M4647</guid>
      <dc:creator>drid</dc:creator>
      <dc:date>2018-04-05T00:48:52Z</dc:date>
    </item>
    <item>
      <title>Re: MMZ09332BT1 R1/R2 for 3.3V / 433MHz</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1-R1-R2-for-3-3V-433MHz/m-p/766660#M4648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;For 3.3V operation, the suggested bias settings:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vcc1 = Vcc2 = Vbias= 3.30 V&lt;BR /&gt;Icc1q = 40 mA, Icc2q = 37 mA&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;R1 510 Ohm&lt;BR /&gt;R2 1000 Ohm&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, change C4=18pF -&amp;gt; 12pF+2.2pF. Other components remain the same as in this schematics.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The resulting small signal gain is 34.5dB, P1dB = 28.2dB @433MHz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Apr 2018 07:47:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1-R1-R2-for-3-3V-433MHz/m-p/766660#M4648</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2018-04-17T07:47:46Z</dc:date>
    </item>
    <item>
      <title>Re: MMZ09332BT1 R1/R2 for 3.3V / 433MHz</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1-R1-R2-for-3-3V-433MHz/m-p/1511043#M13582</link>
      <description>&lt;P&gt;In a post about&amp;nbsp;&lt;SPAN class=""&gt;MMZ25332B you mentioned that you have a&amp;nbsp;&lt;SPAN&gt;guide for adjusting bias resistors with Vdd=5.0V.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Do you have such a guide also for the&amp;nbsp;MMZ09332BT1 for 5V or better in my case 3.3V?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;If so, is it possible to get it?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Thank you in advance&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Thomas&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Aug 2022 15:23:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1-R1-R2-for-3-3V-433MHz/m-p/1511043#M13582</guid>
      <dc:creator>Thomas_</dc:creator>
      <dc:date>2022-08-24T15:23:09Z</dc:date>
    </item>
    <item>
      <title>Re: MMZ09332BT1 R1/R2 for 3.3V / 433MHz</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1-R1-R2-for-3-3V-433MHz/m-p/1519055#M13654</link>
      <description>&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;Can anyone help me with this issue above?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance&lt;/P&gt;</description>
      <pubDate>Thu, 08 Sep 2022 06:54:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/MMZ09332BT1-R1-R2-for-3-3V-433MHz/m-p/1519055#M13654</guid>
      <dc:creator>Thomas_</dc:creator>
      <dc:date>2022-09-08T06:54:20Z</dc:date>
    </item>
  </channel>
</rss>