<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCU中的主题 NHS3152 Flashing</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/NHS3152-Flashing/m-p/1494006#M13442</link>
    <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;We are facing some problem flashing the NHS3152. We bought already 2 NHS3152 ADK dev kits and we were able to flash them using flash magic and LPC-Link2 a couple of time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the first dev&amp;nbsp; kit we lost the ability to flash it after 2 day. The board does not respond and even the device signature is not able to be retrieved&lt;/P&gt;&lt;P&gt;We tested the LPC-link2 with the cable using a NHS3100 dev kit and it was working ok.&lt;/P&gt;&lt;P&gt;So we bought the second NHS3152 ADK. Unfortunately, the same thing happened. After 3 or 4 flashing the device is not responding.&lt;/P&gt;&lt;P&gt;The code that we are trying to develop is just using the ADC in continuous mode based on the NHS31xx SW API – Modules – Drivers – ADCDAC – Example 2&lt;/P&gt;&lt;P&gt;Any suggestion?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
    <pubDate>Fri, 22 Jul 2022 10:45:27 GMT</pubDate>
    <dc:creator>martinsmarco</dc:creator>
    <dc:date>2022-07-22T10:45:27Z</dc:date>
    <item>
      <title>NHS3152 Flashing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NHS3152-Flashing/m-p/1494006#M13442</link>
      <description>&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;We are facing some problem flashing the NHS3152. We bought already 2 NHS3152 ADK dev kits and we were able to flash them using flash magic and LPC-Link2 a couple of time.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;With the first dev&amp;nbsp; kit we lost the ability to flash it after 2 day. The board does not respond and even the device signature is not able to be retrieved&lt;/P&gt;&lt;P&gt;We tested the LPC-link2 with the cable using a NHS3100 dev kit and it was working ok.&lt;/P&gt;&lt;P&gt;So we bought the second NHS3152 ADK. Unfortunately, the same thing happened. After 3 or 4 flashing the device is not responding.&lt;/P&gt;&lt;P&gt;The code that we are trying to develop is just using the ADC in continuous mode based on the NHS31xx SW API – Modules – Drivers – ADCDAC – Example 2&lt;/P&gt;&lt;P&gt;Any suggestion?&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;</description>
      <pubDate>Fri, 22 Jul 2022 10:45:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NHS3152-Flashing/m-p/1494006#M13442</guid>
      <dc:creator>martinsmarco</dc:creator>
      <dc:date>2022-07-22T10:45:27Z</dc:date>
    </item>
    <item>
      <title>Re: NHS3152 Flashing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/NHS3152-Flashing/m-p/1495777#M13464</link>
      <description>&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;Thank you very much for using our products, I'm very sorry that your development board is causing you this issue.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;Do you happen to have a log of the errors that the tool is through while trying to flash the IC?&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial,helvetica,sans-serif" size="3"&gt;This will help us for providing a recommendation or, at least giving us an idea of what could be happening.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jul 2022 18:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/NHS3152-Flashing/m-p/1495777#M13464</guid>
      <dc:creator>Fabian_R</dc:creator>
      <dc:date>2022-07-26T18:19:27Z</dc:date>
    </item>
  </channel>
</rss>