<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: wireless UART &amp;amp; ble</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/wireless-UART-amp-ble/m-p/1486964#M13367</link>
    <description>&lt;P lang="es-MX"&gt;Hi,&lt;/P&gt;
&lt;P lang="es-MX"&gt;Could you please provide more details about your application's connections? Are the connections intended to be like one of the examples in the image below?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EduardoZamora_0-1657303328969.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/186109i5E6F623FA0DD37A3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EduardoZamora_0-1657303328969.png" alt="EduardoZamora_0-1657303328969.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;EduardoZamora_0-1657303328969.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P lang="es-MX"&gt;Please, take a look at Heart Rate Sensor (hrs) and Temperature Sensor (temp_sens) example projects inside the &lt;A href="https://mcuxpresso.nxp.com/en/builder?hw=FRDM-KW38&amp;amp;rel=575" target="_blank"&gt;KW38 SDK&lt;/A&gt; (wireless_examples &amp;gt; bluetooth). These examples could be used as a base to develop your application, they are highly configurable, allowing the user to set some relevant parameters and change the information being transmitted.&lt;/P&gt;
&lt;P&gt;Also, please consult &lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/KW38-Custom-Profile/ta-p/1269874" target="_blank"&gt;KW38 Custom Profile&lt;/A&gt;, you can use this article as a reference for Custom Profile creation as it is needed for both the server and the client GATT services to match.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
    <pubDate>Fri, 08 Jul 2022 18:05:37 GMT</pubDate>
    <dc:creator>EduardoZamora</dc:creator>
    <dc:date>2022-07-08T18:05:37Z</dc:date>
    <item>
      <title>wireless UART &amp; ble</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/wireless-UART-amp-ble/m-p/1486671#M13366</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi, I wanna asking if there is somebody can help me to write a program that can send accelerometer and gyroscopedata using uart and BLE with kw38 MCU Also this program will help the client to choose each type of data ( accelerometer/gyroscope) will be displayed in his device&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(Nanosense sensor)&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jul 2022 07:40:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/wireless-UART-amp-ble/m-p/1486671#M13366</guid>
      <dc:creator>Saoussen</dc:creator>
      <dc:date>2022-07-08T07:40:25Z</dc:date>
    </item>
    <item>
      <title>Re: wireless UART &amp; ble</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/wireless-UART-amp-ble/m-p/1486964#M13367</link>
      <description>&lt;P lang="es-MX"&gt;Hi,&lt;/P&gt;
&lt;P lang="es-MX"&gt;Could you please provide more details about your application's connections? Are the connections intended to be like one of the examples in the image below?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EduardoZamora_0-1657303328969.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/186109i5E6F623FA0DD37A3/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EduardoZamora_0-1657303328969.png" alt="EduardoZamora_0-1657303328969.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;EduardoZamora_0-1657303328969.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P lang="es-MX"&gt;Please, take a look at Heart Rate Sensor (hrs) and Temperature Sensor (temp_sens) example projects inside the &lt;A href="https://mcuxpresso.nxp.com/en/builder?hw=FRDM-KW38&amp;amp;rel=575" target="_blank"&gt;KW38 SDK&lt;/A&gt; (wireless_examples &amp;gt; bluetooth). These examples could be used as a base to develop your application, they are highly configurable, allowing the user to set some relevant parameters and change the information being transmitted.&lt;/P&gt;
&lt;P&gt;Also, please consult &lt;A href="https://community.nxp.com/t5/Wireless-Connectivity-Knowledge/KW38-Custom-Profile/ta-p/1269874" target="_blank"&gt;KW38 Custom Profile&lt;/A&gt;, you can use this article as a reference for Custom Profile creation as it is needed for both the server and the client GATT services to match.&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Eduardo.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Jul 2022 18:05:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/wireless-UART-amp-ble/m-p/1486964#M13367</guid>
      <dc:creator>EduardoZamora</dc:creator>
      <dc:date>2022-07-08T18:05:37Z</dc:date>
    </item>
  </channel>
</rss>