<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic application note AN12657 &amp;quot;Using the RC663 without library&amp;quot; in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/application-note-AN12657-quot-Using-the-RC663-without-library/m-p/1481182#M13326</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hello, I implemented the example 4.2.1 example code - Inventory -ISO15693 of the application note AN12657 about the NFC reader MFRC630 without success. Please, can you clarify step 15 "The function CardResponded reads the IRQ0 register , which indicates if a card has responded or not"? What are the IRQ0 register bits to test? Second point: there is a scripting file for NFC Cockpit to achieve the same result of the example above?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 28 Jun 2022 11:32:55 GMT</pubDate>
    <dc:creator>madid</dc:creator>
    <dc:date>2022-06-28T11:32:55Z</dc:date>
    <item>
      <title>application note AN12657 "Using the RC663 without library"</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/application-note-AN12657-quot-Using-the-RC663-without-library/m-p/1481182#M13326</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hello, I implemented the example 4.2.1 example code - Inventory -ISO15693 of the application note AN12657 about the NFC reader MFRC630 without success. Please, can you clarify step 15 "The function CardResponded reads the IRQ0 register , which indicates if a card has responded or not"? What are the IRQ0 register bits to test? Second point: there is a scripting file for NFC Cockpit to achieve the same result of the example above?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jun 2022 11:32:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/application-note-AN12657-quot-Using-the-RC663-without-library/m-p/1481182#M13326</guid>
      <dc:creator>madid</dc:creator>
      <dc:date>2022-06-28T11:32:55Z</dc:date>
    </item>
    <item>
      <title>Re: application note AN12657 "Using the RC663 without library"</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/application-note-AN12657-quot-Using-the-RC663-without-library/m-p/1483346#M13344</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202918"&gt;@madid&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Please refer to IRQ0 register details,&lt;/P&gt;
&lt;DIV id="tinyMceEditordanielchen_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielchen_1-1656666107891.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/185304i6724081F3095E521/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielchen_1-1656666107891.png" alt="danielchen_1-1656666107891.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielchen_1-1656666107891.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;For how to check CardResponse&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielchen_2-1656666181895.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/185306iAB308669045D2A19/image-size/medium?v=v2&amp;amp;px=400" role="button" title="danielchen_2-1656666181895.png" alt="danielchen_2-1656666181895.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;danielchen_2-1656666181895.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Jul 2022 09:04:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/application-note-AN12657-quot-Using-the-RC663-without-library/m-p/1483346#M13344</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2022-07-01T09:04:01Z</dc:date>
    </item>
    <item>
      <title>Re: application note AN12657 "Using the RC663 without library"</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/application-note-AN12657-quot-Using-the-RC663-without-library/m-p/1485174#M13355</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I did not solve the problem. The interrupt does not trigger; I am very disappointed that an example of an official NXP application does not work&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 08:01:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/application-note-AN12657-quot-Using-the-RC663-without-library/m-p/1485174#M13355</guid>
      <dc:creator>madid</dc:creator>
      <dc:date>2022-07-06T08:01:43Z</dc:date>
    </item>
  </channel>
</rss>