<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックQN9090 based consumer product FCC testing</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-based-consumer-product-FCC-testing/m-p/1460154#M13156</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a custom designed PCB and firmware using the QN9090. The only interface for programming during manufacturing is SWD and once inside a case can't be accessed. No UART available only a LCD display and single button. Is there a source code example of the types of operations required for FCC, such as transmitting on a certain channel. I believe there is a binary that can be used for FCC validation with the DK6 board but since my GPIO is very different and I don't have a UART available this won't work. I need to utilize the LCD and button to setup the various testing modes.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 18 May 2022 15:48:44 GMT</pubDate>
    <dc:creator>alexedge</dc:creator>
    <dc:date>2022-05-18T15:48:44Z</dc:date>
    <item>
      <title>QN9090 based consumer product FCC testing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-based-consumer-product-FCC-testing/m-p/1460154#M13156</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have a custom designed PCB and firmware using the QN9090. The only interface for programming during manufacturing is SWD and once inside a case can't be accessed. No UART available only a LCD display and single button. Is there a source code example of the types of operations required for FCC, such as transmitting on a certain channel. I believe there is a binary that can be used for FCC validation with the DK6 board but since my GPIO is very different and I don't have a UART available this won't work. I need to utilize the LCD and button to setup the various testing modes.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 18 May 2022 15:48:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9090-based-consumer-product-FCC-testing/m-p/1460154#M13156</guid>
      <dc:creator>alexedge</dc:creator>
      <dc:date>2022-05-18T15:48:44Z</dc:date>
    </item>
    <item>
      <title>Re: QN9090 based consumer product FCC testing</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/QN9090-based-consumer-product-FCC-testing/m-p/1461769#M13166</link>
      <description>&lt;P&gt;Hi Alex,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. We have the &lt;A href="https://www.nxp.com/docs/en/nxp/application-notes/AN12610.pdf" target="_blank"&gt;QN9090 RF System Evaluation Report for BLE Applications &lt;/A&gt;(QN9090x_Certi_Tools.bi), but it needs a serial interface, I think this is the example you mentioned.&lt;/P&gt;
&lt;P&gt;This example provides RF evaluation test results of the QN9090 for BLE applications (2FSK modulation).&lt;/P&gt;
&lt;P&gt;You can download the MCUXpresso project from the &lt;A href="https://www.nxp.com/products/wireless/bluetooth-low-energy/qn9090-30-bluetooth-low-energy-mcu-with-armcortex-m4-cpu-energy-efficiency-analog-and-digital-peripherals-and-nfc-tag-option:QN9090-30" target="_blank"&gt;QN9090&lt;/A&gt; page:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="Ricardo_Zamora_1-1653065494086.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/180474i3E7B1597962AF3B2/image-size/large?v=v2&amp;amp;px=999" role="button" title="Ricardo_Zamora_1-1653065494086.png" alt="Ricardo_Zamora_1-1653065494086.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope this helps.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Fri, 20 May 2022 16:52:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/QN9090-based-consumer-product-FCC-testing/m-p/1461769#M13166</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2022-05-20T16:52:00Z</dc:date>
    </item>
  </channel>
</rss>