<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックRe: JN5189 powerdown mode</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1434445#M13020</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Measurements are taken on module power path, but it seems I made a mistake when I left unused pin_10 and pin_11 floating. These are special i2c pins that must have external pull up resistors.&lt;/P&gt;&lt;P&gt;Now after I mount these resistors and configure latching in IOCON registers for two LEDs on my "dev-board", current on one module drops to about 80uA, and on another one to less then 10uA.&lt;/P&gt;&lt;P&gt;Maybe, one module is somehow damaged, I don't know, but this is good enough for me.&lt;/P&gt;&lt;P&gt;Thank you for response.&lt;/P&gt;&lt;P&gt;Damir Serfezi&lt;/P&gt;</description>
    <pubDate>Sun, 27 Mar 2022 12:19:22 GMT</pubDate>
    <dc:creator>Serfa</dc:creator>
    <dc:date>2022-03-27T12:19:22Z</dc:date>
    <item>
      <title>JN5189 powerdown mode</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1430789#M12978</link>
      <description>&lt;P&gt;Hello there&lt;/P&gt;&lt;P&gt;I'm working with Chinese JN5189 module(E180-Z8910SP) and I've got a confusing situation with powerdown mode.&lt;/P&gt;&lt;P&gt;When I run your powerdown example (MCUXpresso IDE -&amp;gt; Quickstart Panel -&amp;gt; Import SDK example(s) -&amp;gt; driver_examples -&amp;gt; powerdown_demo), everything indicates the module is in the powerdown mode, except that I can see there's still too much of current consumption (about 0.7 mA, with no other connections but serial port alone – if there are any pins connected, it further increases).&lt;/P&gt;&lt;P&gt;By the way, deep down mode seems to be working, the consumption is expectedly low.&lt;/P&gt;&lt;P&gt;Could you help me?&lt;/P&gt;&lt;P&gt;Can somebody run the same example and measure the current consumption so I can compare it, because 0.7 mA is definitely too much for the powerdown mode in my opinion.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 18 Mar 2022 16:34:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1430789#M12978</guid>
      <dc:creator>Serfa</dc:creator>
      <dc:date>2022-03-18T16:34:50Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 powerdown mode</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1433669#M13002</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/197165"&gt;@Serfa&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please check the following app note, it mention the expected power consumption using the different power modes:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN12898.pdf" target="_blank"&gt;JN5189-Power Consumption (nxp.com)&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Thu, 24 Mar 2022 22:33:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1433669#M13002</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2022-03-24T22:33:29Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 powerdown mode</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1434197#M13010</link>
      <description>&lt;P&gt;Hi Alexis&lt;/P&gt;&lt;P&gt;Yes, I've seen that pdf, and it is confirmation of what is declared in JN518x data-sheet.&lt;BR /&gt;But could anybody from NXP run example I described in previous post on one of yours dev-boards&lt;BR /&gt;and confirm that JN5189 really enter to power-down mode with current consumption of few dozens uA(microAmpers).&lt;BR /&gt;I like that example as it is super simple, easy to follow and it is about power-down mode.&lt;/P&gt;</description>
      <pubDate>Fri, 25 Mar 2022 14:32:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1434197#M13010</guid>
      <dc:creator>Serfa</dc:creator>
      <dc:date>2022-03-25T14:32:00Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 powerdown mode</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1434311#M13014</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/197165"&gt;@Serfa&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I can confirm the results shown in the application note, and your results seems very high compared to the ones in the datasheet/app note. Are the measurements done only for the module or do you have any other IC connected to that power path?&lt;/P&gt;
&lt;P&gt;BR,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Fri, 25 Mar 2022 22:34:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1434311#M13014</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2022-03-25T22:34:10Z</dc:date>
    </item>
    <item>
      <title>Re: JN5189 powerdown mode</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1434445#M13020</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Measurements are taken on module power path, but it seems I made a mistake when I left unused pin_10 and pin_11 floating. These are special i2c pins that must have external pull up resistors.&lt;/P&gt;&lt;P&gt;Now after I mount these resistors and configure latching in IOCON registers for two LEDs on my "dev-board", current on one module drops to about 80uA, and on another one to less then 10uA.&lt;/P&gt;&lt;P&gt;Maybe, one module is somehow damaged, I don't know, but this is good enough for me.&lt;/P&gt;&lt;P&gt;Thank you for response.&lt;/P&gt;&lt;P&gt;Damir Serfezi&lt;/P&gt;</description>
      <pubDate>Sun, 27 Mar 2022 12:19:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/JN5189-powerdown-mode/m-p/1434445#M13020</guid>
      <dc:creator>Serfa</dc:creator>
      <dc:date>2022-03-27T12:19:22Z</dc:date>
    </item>
  </channel>
</rss>