<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN7150 working without battery. in Wireless MCU</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/PN7150-working-without-battery/m-p/1428573#M12965</link>
    <description>&lt;P&gt;Hi.&lt;BR /&gt;&lt;BR /&gt;I'm developing a PCB circuit with a microcontroller and the NFC PN7150.&lt;/P&gt;&lt;P&gt;My hardware doesn't need a battery to work, so my question is:&lt;BR /&gt;&lt;BR /&gt;Do the battery related pins VBAT1, VBAT2 and VBAT need to be connected to a 5V source or can they be left unused?&lt;/P&gt;&lt;P&gt;I can't find any information on that subject, so it is assumed that there will always be a backup battery.&lt;/P&gt;&lt;P&gt;Any comment or suggestion is welcome&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 15 Mar 2022 14:16:24 GMT</pubDate>
    <dc:creator>dominusdrr</dc:creator>
    <dc:date>2022-03-15T14:16:24Z</dc:date>
    <item>
      <title>PN7150 working without battery.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN7150-working-without-battery/m-p/1428573#M12965</link>
      <description>&lt;P&gt;Hi.&lt;BR /&gt;&lt;BR /&gt;I'm developing a PCB circuit with a microcontroller and the NFC PN7150.&lt;/P&gt;&lt;P&gt;My hardware doesn't need a battery to work, so my question is:&lt;BR /&gt;&lt;BR /&gt;Do the battery related pins VBAT1, VBAT2 and VBAT need to be connected to a 5V source or can they be left unused?&lt;/P&gt;&lt;P&gt;I can't find any information on that subject, so it is assumed that there will always be a backup battery.&lt;/P&gt;&lt;P&gt;Any comment or suggestion is welcome&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Mar 2022 14:16:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN7150-working-without-battery/m-p/1428573#M12965</guid>
      <dc:creator>dominusdrr</dc:creator>
      <dc:date>2022-03-15T14:16:24Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 working without battery.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN7150-working-without-battery/m-p/1428845#M12966</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/156216"&gt;@dominusdrr&lt;/a&gt;&amp;nbsp;.&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP technical support.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;gt;&amp;gt; Do the battery related pins VBAT1, VBAT2 and VBAT need to be connected to a 5V source or can they be left unused?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Need to be connected to&amp;nbsp; a 5V source.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Please kindly refer to the&amp;nbsp;12.5.3.2 Configuration 2: supply connection in case a 5 V supply is used to generate RF field with the use of TXLDO of the datasheet as the link.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;URL:&lt;A href="https://www.nxp.com/docs/en/data-sheet/PN7150.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/PN7150.pdf&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 01:46:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN7150-working-without-battery/m-p/1428845#M12966</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2022-03-16T01:46:55Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 working without battery.</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN7150-working-without-battery/m-p/1429338#M12970</link>
      <description>&lt;P&gt;Hi.&lt;BR /&gt;&lt;BR /&gt;Thanks for your help.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Mar 2022 13:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN7150-working-without-battery/m-p/1429338#M12970</guid>
      <dc:creator>dominusdrr</dc:creator>
      <dc:date>2022-03-16T13:52:06Z</dc:date>
    </item>
  </channel>
</rss>