<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Wireless MCUのトピックPN512 RX circuit design</title>
    <link>https://community.nxp.com/t5/Wireless-MCU/PN512-RX-circuit-design/m-p/1422629#M12935</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we have a PN512 chip for read the NFC tags on a device that we acquire from an our partner. I don0't have the schematics but i have done a short reverse engineering. We have some problems on the RX circuit, many time the card is not correctly readed.&lt;/P&gt;&lt;P&gt;I have seen on different application note that the rx circuit for the PN512 is proposed in two different ways:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;circuit 1 and 2 from&amp;nbsp;Blueboard_PNEV512B_v1.5_SCH and AN1445&lt;/LI&gt;&lt;LI&gt;circuit 3 from AN11038&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;in our case the circuit implemented is the circuit 3. If i switch from the circuit 3 to the circuit 1 (inverting R1 with C3) the reader seems to work better.&lt;/P&gt;&lt;P&gt;What are the difference between the two circuit? Which is the best? or are equivalent?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 03 Mar 2022 10:33:43 GMT</pubDate>
    <dc:creator>dc1</dc:creator>
    <dc:date>2022-03-03T10:33:43Z</dc:date>
    <item>
      <title>PN512 RX circuit design</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN512-RX-circuit-design/m-p/1422629#M12935</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we have a PN512 chip for read the NFC tags on a device that we acquire from an our partner. I don0't have the schematics but i have done a short reverse engineering. We have some problems on the RX circuit, many time the card is not correctly readed.&lt;/P&gt;&lt;P&gt;I have seen on different application note that the rx circuit for the PN512 is proposed in two different ways:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;circuit 1 and 2 from&amp;nbsp;Blueboard_PNEV512B_v1.5_SCH and AN1445&lt;/LI&gt;&lt;LI&gt;circuit 3 from AN11038&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;in our case the circuit implemented is the circuit 3. If i switch from the circuit 3 to the circuit 1 (inverting R1 with C3) the reader seems to work better.&lt;/P&gt;&lt;P&gt;What are the difference between the two circuit? Which is the best? or are equivalent?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Mar 2022 10:33:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN512-RX-circuit-design/m-p/1422629#M12935</guid>
      <dc:creator>dc1</dc:creator>
      <dc:date>2022-03-03T10:33:43Z</dc:date>
    </item>
    <item>
      <title>Re: PN512 RX circuit design</title>
      <link>https://community.nxp.com/t5/Wireless-MCU/PN512-RX-circuit-design/m-p/1423605#M12943</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/143910"&gt;@dc1&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your information.&lt;/P&gt;
&lt;P&gt;The principle of receiver circuit please kindly refer to 4.6 Receiver circuit design of AN1445.&lt;BR /&gt;circuit 3 and 2 are the reference design. circuit 1 is the design of the development board which is verified by NXP. So we recommend the customer to follow the design if have the same antenna size.&lt;/P&gt;
&lt;P&gt;Have a nice day.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-----------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Mon, 07 Mar 2022 02:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Wireless-MCU/PN512-RX-circuit-design/m-p/1423605#M12943</guid>
      <dc:creator>fangfang</dc:creator>
      <dc:date>2022-03-07T02:25:32Z</dc:date>
    </item>
  </channel>
</rss>